STM32U575QII Dedicated OPAMP2_VINM pin not connected?
I have a project which uses both OPAMPs. For both OA I use dedicated VINM pin.
OPAMP1 works correctly.
OPAMP2 behaves like the dedicated pin (M2 ball) is not connected to the input multiplexer.
I 've tried
- mode FOLLOWER: OK
- mode STANDALONE, reconnected the signal on the board and used PA7 for VINM: OK
- mode STANDALONE, using the dedicated pin: the output is saturated at VDDA.
Checked the PCB connection, OK. Checked on 3 boards, identical results.
Is it possible it is really a bug in the silicon? What else should I check?
(I would like to use OPAMP tag, but it is not available :( )
Initialization code:
(GPIO to analog)
LL_APB3_GRP1_EnableClock(LL_APB3_GRP1_PERIPH_OPAMP);
LL_OPAMP_InitTypeDef OPAMP_Init;
OPAMP_Init.PowerMode = LL_OPAMP_POWERMODE_NORMALPOWER_NORMALSPEED;
OPAMP_Init.FunctionalMode = LL_OPAMP_MODE_STANDALONE;
OPAMP_Init.InputNonInverting = LL_OPAMP_INPUT_NONINVERT_IO0;
OPAMP_Init.InputInverting = LL_OPAMP_INPUT_INVERT_IO1;
LL_OPAMP_Init(OPAMP2, &OPAMP_Init);
LL_OPAMP_Enable(OPAMP2);