Skip to main content
Visitor II
February 4, 2025
Solved

STM32U575RGT6 without UCPD

  • February 4, 2025
  • 2 replies
  • 440 views

Hi,
We're in the process of developing a new board and I've got a question about USB.

We would like to have a USB device with MSC only.

Can we not activate the UCPD and work with the TCPP01-M12 FLT, DB CC1 and CC2 signals at ground (as on the STM32U545 eval kit)?

At the moment, I can't get the USB to work without the UCPD enabled on the NUCLEO-U575ZI-Q board.

    This topic has been closed for replies.
    Best answer by Mickael_Biyotee

    Hello,
    I could not get the USB device to work without the TCPP01-M12 FLT, DB CC1 and CC2 signals.
    I have modified my hardware to drive the signals as on the NUCLEO-U575ZI-Q board.
    thank you for your feedback.

    2 replies

    ST Employee
    February 5, 2025

    Your question:

    We would like to have a USB device with MSC only.

    Can we not activate the UCPD and work with the TCPP01-M12 FLT, DB CC1 and CC2 signals at ground (as on the STM32U545 eval kit)?

     

    I think it is OK to have a USB device with MSC to work without UCPD (UCPD pins floating).

     

    Mickael_BiyoteeAuthorAnswer
    Visitor II
    February 12, 2025

    Hello,
    I could not get the USB device to work without the TCPP01-M12 FLT, DB CC1 and CC2 signals.
    I have modified my hardware to drive the signals as on the NUCLEO-U575ZI-Q board.
    thank you for your feedback.