STM32U575ZIT6 USB FS problem
Hello all, i got a firmware configuration problem,
basically im using USB in FS modem and when i plug in the usb to the pc what happens is that sometimes it can be recognized and i see a network disk called ''boot'' but most of times it cant be recognized, so i gotta power up again the whole circuit until it can be seen, i thought it would be a frequency problem, but i already saw that configuration is set to 48MHz , so its correct, i added also a delay before initialization of the usb but it still doesnt work, what else i can try? can someone give me some tips? i already read on many forums but still didnt find out