STM32U585 need help with getting ADC -> DMA working in trivial case.
This is what I am doing and want to accomplish:
I am using ADC4 to convert internal temperature sensor in 1 second intervals, and move the converted value from ADC_DR register to a fixed address in RAM (no increment). At the end, I want to be able to watch one RAM address in debug mode memory browser and see its value change every 1 second.
ALREADY HAVE THE FOLLOWING WORKING:
TIM2 timer is triggering ACD4 every 1 second, and ADC4 is placing the converted value to ADC_DR register. I am able to observer the value using the EOC interrupt when reading ADC_DR value in interrupt handler.
I CANNOT GET THIS WORKING:
When I incorporate GPDMA and select source as ADC_DR register and destination as , for example, 0x20000008U address. I cannot see any values places at this RAM address.
(Note: I stop reading the ADC_DR register value in the EOC interrupt handler so the converted value can be picked up by GPDMA.)
I NEED HELP with figuring out what other registers and register values I need to set/clear to get GPDMA working.
Here is what I have so far:
(Note: No HAL, No LL. The following are my functions defined in assembly language where each function sets/clears appropriate bits of a register, based on reference manual and datasheet.)
1. To integrate GPDMA on ADC4, I:
ADC4_DMAEN_Mode_Enable();
ADC4_DMACFG_Circular_Set();
ADC4_Set_Single(); //Set single conversion mode so on each timer update it does one conversion.
1. To configure GPDMA, I do the following:
RCC_DMA_Set_Clock();
DMA_SECCFGR_Set_Nonsecure();
DMA_PRIVCFGR_Set_Unprivileged();
DMA_C0SAR_Set_Source(); //ADC_DR register address 0x46021040U
DMA_C0DAR_Set_Destination(); //0x20000008U
DMA_C0TR1_Set_DestInc_Fixed();
DMA_C0TR1_Set_SrcInc_Fixed();
DMA_C0BR1_Set_NumOfItemsInBlockToTransfer(); //2 for 2 bytes, 16bits as ADC_DR is 16bits
DMA_C0TR1_Set_SBL_1_Burst_Lenght(); //set to 0
DMA_C0TR1_Set_SDW_LOG2_Source_Block_Size(); //set to 1
DMA_C0TR1_Set_DBL_1_Set_Burst_Lenght(); //set to 0
DMA_C0TR1_Set_DDW_LOG2_Dest_Block_Size(); //set to 1
DMA_C0CR_Set_Interrupts();
NVIC_DMA_Enable_Interupt();
DMA_C0CR_Set_Enable();
What other registers and register values I need to set/clear for GPDMA to work for the scenario?