STM32U599 OC Tim DMA failed start or do some toggle
We try generate signal defined by toggle table , but command do nothink. (except ARR toggles)
if (HAL_TIM_OC_Start_DMA(&htim2, TIM_CHANNEL_4, &tim_values[0], idx) != HAL_OK)
{
Error_Handler();
}have 1.7.0 U5 firmware some known issue ? Or what is required to right setup this.
We try add enable GPDMA etc. No change. For ARR is one toggle no based on table. Seems we skip some trigger setup or U5 HAL is buggy .? Pls help. Simply we have table and require toggle for example 20 words table in time.
Actual config:
main ...
/* Initialize all configured peripherals */
MX_GPDMA1_Init();
MX_CRC_Init();
MX_RAMCFG_Init();
MX_DSIHOST_DSI_Init();
MX_LTDC_Init();
MX_TIM3_Init();
MX_USART2_UART_Init();
MX_DCACHE1_Init();
MX_ICACHE_Init();
MX_DMA2D_Init();
MX_GPU2D_Init();
MX_DCACHE2_Init();
MX_TIM2_Init();
MX_TouchGFX_Init();
/* Call PreOsInit function */
static void MX_TIM2_Init(void)
{
/* USER CODE BEGIN TIM2_Init 0 */
/* USER CODE END TIM2_Init 0 */
TIM_ClockConfigTypeDef sClockSourceConfig = {0};
TIM_MasterConfigTypeDef sMasterConfig = {0};
TIM_OC_InitTypeDef sConfigOC = {0};
/* USER CODE BEGIN TIM2_Init 1 */
/* USER CODE END TIM2_Init 1 */
htim2.Instance = TIM2;
htim2.Init.Prescaler = 159;
htim2.Init.CounterMode = TIM_COUNTERMODE_UP;
htim2.Init.Period = 1000000; //4294967295;
htim2.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
htim2.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
if (HAL_TIM_Base_Init(&htim2) != HAL_OK)
{
Error_Handler();
}
sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
if (HAL_TIM_ConfigClockSource(&htim2, &sClockSourceConfig) != HAL_OK)
{
Error_Handler();
}
if (HAL_TIM_OC_Init(&htim2) != HAL_OK)
{
Error_Handler();
}
sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;
sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
if (HAL_TIMEx_MasterConfigSynchronization(&htim2, &sMasterConfig) != HAL_OK)
{
Error_Handler();
}
sConfigOC.OCMode = TIM_OCMODE_TOGGLE;
sConfigOC.Pulse = 0;
sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH;
sConfigOC.OCFastMode = TIM_OCFAST_DISABLE;
if (HAL_TIM_OC_ConfigChannel(&htim2, &sConfigOC, TIM_CHANNEL_4) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN TIM2_Init 2 */
// HAL_TIM_OC_Start(&htim2,TIM_CHANNEL_4);
/* USER CODE END TIM2_Init 2 */
HAL_TIM_MspPostInit(&htim2);
}
void HAL_TIM_Base_MspInit(TIM_HandleTypeDef* htim_base)
{
if(htim_base->Instance==TIM2)
{
/* USER CODE BEGIN TIM2_MspInit 0 */
/* USER CODE END TIM2_MspInit 0 */
/* Peripheral clock enable */
__HAL_RCC_TIM2_CLK_ENABLE();
/* TIM2 DMA Init */
/* GPDMA1_REQUEST_TIM2_CH4 Init */
handle_GPDMA1_Channel0.Instance = GPDMA1_Channel0;
handle_GPDMA1_Channel0.Init.Request = GPDMA1_REQUEST_TIM2_CH4;
handle_GPDMA1_Channel0.Init.BlkHWRequest = DMA_BREQ_SINGLE_BURST;
handle_GPDMA1_Channel0.Init.Direction = DMA_MEMORY_TO_PERIPH;
handle_GPDMA1_Channel0.Init.SrcInc = DMA_SINC_INCREMENTED;
handle_GPDMA1_Channel0.Init.DestInc = DMA_DINC_FIXED;
handle_GPDMA1_Channel0.Init.SrcDataWidth = DMA_SRC_DATAWIDTH_WORD;
handle_GPDMA1_Channel0.Init.DestDataWidth = DMA_DEST_DATAWIDTH_WORD;
handle_GPDMA1_Channel0.Init.Priority = DMA_LOW_PRIORITY_HIGH_WEIGHT;
handle_GPDMA1_Channel0.Init.SrcBurstLength = 1;
handle_GPDMA1_Channel0.Init.DestBurstLength = 1;
handle_GPDMA1_Channel0.Init.TransferAllocatedPort = DMA_SRC_ALLOCATED_PORT0|DMA_DEST_ALLOCATED_PORT0;
handle_GPDMA1_Channel0.Init.TransferEventMode = DMA_TCEM_BLOCK_TRANSFER;
handle_GPDMA1_Channel0.Init.Mode = DMA_NORMAL;
if (HAL_DMA_Init(&handle_GPDMA1_Channel0) != HAL_OK)
{
Error_Handler();
}
__HAL_LINKDMA(htim_base, hdma[TIM_DMA_ID_CC4], handle_GPDMA1_Channel0);
if (HAL_DMA_ConfigChannelAttributes(&handle_GPDMA1_Channel0, DMA_CHANNEL_NPRIV) != HAL_OK)
{
Error_Handler();
}
/* TIM2 interrupt Init */
HAL_NVIC_SetPriority(TIM2_IRQn, 5, 0);
HAL_NVIC_EnableIRQ(TIM2_IRQn);
/* USER CODE BEGIN TIM2_MspInit 1 */
LL_DMA_EnableChannel(GPDMA1,LL_DMA_CHANNEL_0);
/* USER CODE END TIM2_MspInit 1 */
}
else if(htim_base->Instance==TIM3)
{
/* USER CODE BEGIN TIM3_MspInit 0 */
/* USER CODE END TIM3_MspInit 0 */
/* Peripheral clock enable */
__HAL_RCC_TIM3_CLK_ENABLE();
/* USER CODE BEGIN TIM3_MspInit 1 */
/* USER CODE END TIM3_MspInit 1 */
}
else if(htim_base->Instance==TIM15)
{
/* USER CODE BEGIN TIM15_MspInit 0 */
/* USER CODE END TIM15_MspInit 0 */
/* Peripheral clock enable */
__HAL_RCC_TIM15_CLK_ENABLE();
/* USER CODE BEGIN TIM15_MspInit 1 */
/* USER CODE END TIM15_MspInit 1 */
}
}void HAL_TIM_MspPostInit(TIM_HandleTypeDef* htim)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
if(htim->Instance==TIM2)
{
/* USER CODE BEGIN TIM2_MspPostInit 0 */
/* USER CODE END TIM2_MspPostInit 0 */
__HAL_RCC_GPIOB_CLK_ENABLE();
/**TIM2 GPIO Configuration
PB11 ------> TIM2_CH4
*/
GPIO_InitStruct.Pin = OC_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_AF_OD;
GPIO_InitStruct.Pull = GPIO_PULLUP;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF1_TIM2;
HAL_GPIO_Init(OC_GPIO_Port, &GPIO_InitStruct);
/* USER CODE BEGIN TIM2_MspPostInit 1 */
/* USER CODE END TIM2_MspPostInit 1 */
}
else if(htim->Instance==TIM3)
{
/* USER CODE BEGIN TIM3_MspPostInit 0 */
/* USER CODE END TIM3_MspPostInit 0 */
__HAL_RCC_GPIOE_CLK_ENABLE();
/**TIM3 GPIO Configuration
PE3 ------> TIM3_CH1
*/
GPIO_InitStruct.Pin = LCD_LED_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
GPIO_InitStruct.Alternate = GPIO_AF2_TIM3;
HAL_GPIO_Init(LCD_LED_GPIO_Port, &GPIO_InitStruct);
/* USER CODE BEGIN TIM3_MspPostInit 1 */
/* USER CODE END TIM3_MspPostInit 1 */
}
}