STM32U599ZJT Bootloader Stuck in Reset Loop - STM32 Bootloader
Hello Everyone!
I am facing an issue while trying to enter the STM32 bootloader via USART1 on an STM32U599ZJT.
Issue:
When applying 3.3V to BOOT0 and performing a single reset, the MCU enters a reset (boot?) loop, which persists until BOOT0 is deasserted.
Test Case:
- BOOT0 → 3.3V
- NRST pulled to GND once (manual reset)
- MCU stuck in a reset loop (observed reset pulses on NRST, ~50-120 ms period)
However, when BOOT0 → GND, the reset loop stops, and the MCU behaves normally.
Additional Information:
- Custom PCB
- Following AN2606 guidelines
- Reference test performed successfully on an STM32G0
Any insights on what might be causing this behavior would be greatly appreciated!
Thank you in advance for your help!