STM32U5A5 Hard fault setting SYSCLK > 64Mhz
I'm trying to crank up the clock to Timer1 to be able to count high frequency events with better resolution. If I set the SYSCLK to 128 I get a hard fault when my code reaches SystemClock_Config(). Even if I keep the AHB bus at the same speed (64Mhz) using prescaler. In this case the only clock difference seems to be SYSCLK value.
Here's the first configuration which works ok:

and here's the other where it will hard fault:

Since the IDE says I should be able to take HCLK to 160Mhz which would require a much higher SYSCLK, I don't see why this SYSCLK value should cause a fault.