STM32U5A5: OCTOSPI and 1.08V GPIOs
In datasheet for STM32U5Axx is mentioned:
a) "up to 14 I/Os with independent supply down to 1.08 V" - cool, great feature I need
b) OCTOSPIM: "efficient OCTOSPI pin assignment with a full I/O matrix (before alternate function map)"
What does it mean?
Could I route OCTOSPI signals to 1.08V GPIO? (which I would need)
When I check which of the GPIOs are 1.08V - I do not see a complete QOCTOSPI pin ALT setting possible on it.
But could I bring a Quad-SPI signal set out on the 1.08V GPIOs (setting it to 1.2V)?