Skip to main content
Visitor II
December 23, 2024
Question

STM32U5A5QJI6Q - Which Pins to Use for Programming ?

  • December 23, 2024
  • 2 replies
  • 668 views

Hi,

I am working with the STM32U5A5QJI6Q microcontroller and need guidance on the programming pins. I plan to program it using [SWD/JTAG (choose one)] with an external programmer like ST-Link.

Could someone confirm:

  1. Which pins are used for programming via [SWD/JTAG]?
  2. Are there any specific configurations or settings I need to enable in the hardware or firmware for successful programming?
  3. If using the internal bootloader, what are the required connections (e.g., UART or USB pins)?

I am currently working on a project that incorporates the STM32U5A5QJI6Q microcontroller, and I would like to request the official reference design or any relevant design resources for this specific part. Having access to a detailed reference design would greatly assist in ensuring an optimal hardware implementation.

Any reference to the datasheet or specific examples would be greatly appreciated.

Thank you!

Sathiya

    This topic has been closed for replies.

    2 replies

    Graduate II
    December 23, 2024

    For SWD, minimally PA13/PA14, read the Data Sheet

    For System Loader options, review Application Note AN2606

    For a Schematic, go to the "CAD Resources" tab for NUCLEO, DISCO, or EVAL boards

    Super User
    December 23, 2024