STM32U5A9: Unable to set RTC_CR WUTIE and WUTE bits
Hello,
We are using the RTC wakeup timer and I have noticed that sometimes the WUTIE and WUTE bits are not being set. We are using HAL_RTCEx_SetWakeUpTimer_IT() HAL function to enable the timer. In stepping through the HAL code, it sets the RTC_CR_WUTIE and RTC_CR_WUTE bits but does not check they are actually set, so I assume it is expected to set the bits.
I have read through the reference manual (RM0456) and existing errata. There is no existing errata w.r.t the RTC unit that applies to this situation.
Any insight would be appreciated.
Thanks,
Aidan