STM32U5A9J-DK1 USB Device question
I'm attempting to implement a USB MSC Device using the USB_OTG_HS on a STM32U5A9J-DK1. I'm using the STM32CubeMX version 6.14.1 and STM32Cube_FW_U5_V1.7.0 to create a USBX stand-alone (without THREADX) MSC device. The project builds and runs, with successful initialization of the USBX device subsystem. However, connecting to a host does not trigger the OTG_HS_IRQHandler() interrupt. A couple of questions:
A call to MX_USB_OTG_HS_PCD_Init() is generated in main by CubeMX, but I don't find anywhere in the code where PA11 and PA12 are initialized to the USB_OTG_HS alternate functions.
Since enabling VBUS Sensing via PA9 is not an available option for this device in the CubeMX, and I see from the schematic that VBUS_SENSE is connected to PG1, I'm not at all clear how connection to a host is detected to fire the USB_OTG_HS interrupt.
The STM32Cube_FW_U5 only contains examples for USBX Host, so I'm not sure where to look for guidance.