STM32U5G7VJT6Q - 5V-tolerant pins (FT_h) for Hall encoder
Hi,
MCU planned to use - STM32U5G7VJT6Q
Planning to use PD12,PD13,PE0,PE3,PC7,PE5 as encoder and hall sensor pins as shown below in the image.
But these signals are 5V logic. Is it okay if we give 5V to these pins?
In datasheet it is mentioned as 5V tolerant pins(FT_h). Does it affect its performance? any AC/ DC characteristic issue will rise because of this. Please confirm.
Or suggest which pins can be used or any other alternate way. Also the possible failure cases.