stm32u5g9,zephyr, low power manager
Hi,
I'm using the Zephyr platform with the STM32U5G9ZJ-DK2 board. I want to put the device into a low-power mode when it's not working. After modifying the DTS file and enabling power management, the device can enter and wake up from Stop3 mode normally. However, according to the datasheet, all IOs are in a floating state in Stop3 mode, but I need to control peripheral devices through some IOs. Is there any way for me to handle these IOs when entering and exiting Stop3, or can I choose to enter only Stop2 mode?
Yang,
BR