STM32U5G9ZJT6Q: three displays (two SPI and one 24 RGB)
Hi, good morning to all. I'm in the process to design an application based on STM32U5G9ZJT6Q. My first question, please, is: is it possible to have this STM32 drive three different displays, and possibly have TouchGFX manage the whole three ?
In my case I've:
- Display #1: Rotary 1.3" display (SPI interface, 240x240. IC GC9A01N). Connected to:
- STM32's SPI3-MOSI
- STM32's SPI3-SCK
- STM32's general GPIOs for Chip Select and D/C Select
- Display #2: Same type Rotary 1.3" display (SPI interface, 240x240. IC GC9A01N). Connected to:
- STM32's SPI1-MOSI
- STM32's SPI1-SCK
- STM32's general GPIOs for Chip Select and D/C Select
- Display #3: 5" display (24 bit RGB interface, 800x480. IC ST7262-G4). Touch screen for user selection options. Connected to the STM32's dedicated 8xR, 8XG, 8XB, plus VSYNC, HSYNC, etc.
Would this work ?
Furthermore, second question, sorry: if I utilize MOSI and SCK dedicated pins on the STM32 (on SPI1 for example), can I utilize the other SPI1's pins of the same interface for other 'generic' applications (MISO, RDY, NSS pins, which I don't plan to utilize for SPI interface) ?.
Thank you so much in advance !
Cheers, a good day
Matteo