STMF4 External interrupt → DMA 20-bit SPI xfer → completion interrupt to ISR
Background, using STM32F412CG:
- we have an external 20-bit ADC triggered by an external conversion strobe
- the ADC produces a signal when conversion is complete
- external ADC-complete signal must trigger DMA to read the ADC results (20-bit over SPI)
- DMA-completion of SPI xfer must trigger a transfer-complete interrupt (enter ISR after data received&ready)
I’ve done this with several other vendors’ parts but I’m a newbie to the STM family, so a few questions:
- I read application note AN4031 on DMA controller use, but I don’t see from this note how DMA can be triggered from an external pin? Any recommended example?
- How does the 16-bit SPI do a 20-bit transfer using DMA, and trigger an interrupt on completion? (SPI transfers >16-bit are very common so this must be possible)? Recommended examples?
Thanks in advance for any pointers,
Best Regards, Dave