STMF407G-DISC1 LED are not changing in project, despite value changing correctly
Hello,
I made simpler project, where led is switched on button to represent binary, and there it works. Two RNG values (0-7 and 8-15) are generated and with button press switches between LED binary representation of two RNG values.
I made the same thing in main project and it don't work there. If first RNG number is 6 or 7 it work fine, but 0 to 5 LED dont change to other number.
I debuged it and the values are changing correctly, checked memory in Build Analiser and its fine there too, i have DSP filters there that change to same value and they works fine. What could be the reason why it dont work now.
main project:
/* USER CODE BEGIN Header */
/**
******************************************************************************
* @file : main.c
* @brief : Main program body
******************************************************************************
* @attention
*
* <h2><center>© Copyright (c) 2019 STMicroelectronics.
* All rights reserved.</center></h2>
*
* This software component is licensed by ST under Ultimate Liberty license
* SLA0044, the "License"; You may not use this file except in compliance with
* the License. You may obtain a copy of the License at:
* www.st.com/SLA0044
*
******************************************************************************
*/
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"
#include "filter_coef.h"
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
/* USER CODE END Includes */
/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */
/* USER CODE END PTD */
/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
/* USER CODE END PD */
/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */
/* USER CODE END PM */
/* Private variables ---------------------------------------------------------*/
I2S_HandleTypeDef hi2s2;
DMA_HandleTypeDef hdma_i2s2_ext_rx;
DMA_HandleTypeDef hdma_spi2_tx;
/* USER CODE BEGIN PV */
uint16_t mode=0;
uint16_t fa=0;
uint32_t f1=0;
uint32_t f2=0;
RNG_HandleTypeDef hrng;
/* USER CODE END PV */
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_RNG_Init(void);
static void MX_DMA_Init(void);
static void MX_I2S2_Init(void);
uint16_t rxBuf[8];
uint16_t txBuf[8];
static float firdata1 [FILTER_TAP_NUM1];
static int firptr1 [FILTER_TAP_NUM1];
static int fir_w_ptr1=0;
static float firdata2 [FILTER_TAP_NUM2];
static int firptr2 [FILTER_TAP_NUM2];
static int fir_w_ptr2=0;
static float firdata3 [FILTER_TAP_NUM3];
static int firptr3 [FILTER_TAP_NUM3];
static int fir_w_ptr3=0;
static float firdata4 [FILTER_TAP_NUM4];
static int firptr4 [FILTER_TAP_NUM4];
static int fir_w_ptr4=0;
static float firdata5 [FILTER_TAP_NUM5];
static int firptr5 [FILTER_TAP_NUM5];
static int fir_w_ptr5=0;
static float firdata6 [FILTER_TAP_NUM6];
static int firptr6 [FILTER_TAP_NUM6];
static int fir_w_ptr6=0;
static float firdata9 [FILTER_TAP_NUM9];
static int firptr9 [FILTER_TAP_NUM9];
static int fir_w_ptr9=0;
static float firdata10 [FILTER_TAP_NUM10];
static int firptr10 [FILTER_TAP_NUM10];
static int fir_w_ptr10=0;
static float firdata11 [FILTER_TAP_NUM11];
static int firptr11 [FILTER_TAP_NUM11];
static int fir_w_ptr11=0;
static float firdata12 [FILTER_TAP_NUM12];
static int firptr12 [FILTER_TAP_NUM12];
static int fir_w_ptr12=0;
static float firdata13 [FILTER_TAP_NUM13];
static int firptr13 [FILTER_TAP_NUM13];
static int fir_w_ptr13=0;
static float firdata14 [FILTER_TAP_NUM14];
static int firptr14 [FILTER_TAP_NUM14];
static int fir_w_ptr14=0;
static float firdata15 [FILTER_TAP_NUM15];
static int firptr15 [FILTER_TAP_NUM15];
static int fir_w_ptr15=0;
static float firdata16 [FILTER_TAP_NUM16];
static int firptr16 [FILTER_TAP_NUM16];
static int fir_w_ptr16=0;
int main(void)
{
HAL_Init();
SystemClock_Config();
MX_GPIO_Init();
MX_DMA_Init();
MX_RNG_Init();
MX_I2S2_Init();
HAL_I2SEx_TransmitReceive_DMA (&hi2s2, txBuf, rxBuf, 4);
HAL_RNG_GenerateRandomNumber(&hrng,&f1);
f1=f1%8;
//f2=f1+8;
HAL_RNG_GenerateRandomNumber(&hrng,&f2);
f2=(f2%8)+8;
mode=f1;
while (1)
{
if(mode == 0){
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12, GPIO_PIN_RESET);
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13, GPIO_PIN_RESET);
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_14, GPIO_PIN_RESET);
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_RESET);}
if(mode == 1){
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12, GPIO_PIN_SET);
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13, GPIO_PIN_RESET);
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_14, GPIO_PIN_RESET);
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_RESET);}
if(mode == 2){
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12, GPIO_PIN_RESET);
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13, GPIO_PIN_SET);
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_14, GPIO_PIN_RESET);
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_RESET);}
if(mode == 3){
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12, GPIO_PIN_SET);
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13, GPIO_PIN_SET);
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_14, GPIO_PIN_RESET);
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_RESET);}
if(mode == 4){
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12, GPIO_PIN_RESET);
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13, GPIO_PIN_RESET);
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_14, GPIO_PIN_SET);
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_RESET);}
if(mode == 5){
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12, GPIO_PIN_SET);
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13, GPIO_PIN_RESET);
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_14, GPIO_PIN_SET);
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_RESET);}
if(mode == 6){
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12, GPIO_PIN_RESET);
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13, GPIO_PIN_SET);
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_14, GPIO_PIN_SET);
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_RESET);}
if(mode == 7){
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12, GPIO_PIN_SET);
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13, GPIO_PIN_SET);
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_14, GPIO_PIN_SET);
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_RESET);}
if(mode == 8){
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12, GPIO_PIN_RESET);
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13, GPIO_PIN_RESET);
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_14, GPIO_PIN_RESET);
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_SET);}
if(mode == 9){
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12, GPIO_PIN_SET);
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13, GPIO_PIN_RESET);
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_14, GPIO_PIN_RESET);
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_SET);}
if(mode == 10){
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12, GPIO_PIN_RESET);
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13, GPIO_PIN_SET);
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_14, GPIO_PIN_RESET);
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_SET);}
if(mode == 11){
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12, GPIO_PIN_SET);
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13, GPIO_PIN_SET);
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_14, GPIO_PIN_RESET);
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_SET);}
if(mode == 12){
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12, GPIO_PIN_RESET);
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13, GPIO_PIN_RESET);
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_14, GPIO_PIN_SET);
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_SET);}
if(mode == 13){
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12, GPIO_PIN_SET);
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13, GPIO_PIN_RESET);
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_14, GPIO_PIN_SET);
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_SET);}
if(mode == 14){
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12, GPIO_PIN_RESET);
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13, GPIO_PIN_SET);
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_14, GPIO_PIN_SET);
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_SET);}
if(mode == 15){
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12, GPIO_PIN_SET);
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13, GPIO_PIN_SET);
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_14, GPIO_PIN_SET);
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_SET);}
}
}
void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin)
{
fa=fa+1;
if(fa>1)
fa=0;
if(fa==0)
mode=f1;
if(fa==1)
mode=f2;
}
int Calc_FIR1 (int inSample) {
float inSampleF = (float)inSample;
float outdata = 0;
for (int i=0;i < FILTER_TAP_NUM1; i++) {
outdata += (firdata1[i]*filter_taps1[firptr1[i]]);
firptr1[i]++;
}
firdata1[fir_w_ptr1] = inSampleF;
firptr1[fir_w_ptr1] = 0;
fir_w_ptr1++;
if (fir_w_ptr1 == FILTER_TAP_NUM1) fir_w_ptr1=0;
return (int) outdata;
}
int Calc_FIR2 (int inSample) {
float inSampleF = (float)inSample;
float outdata = 0;
for (int i=0;i < FILTER_TAP_NUM2; i++) {
outdata += (firdata2[i]*filter_taps2[firptr2[i]]);
firptr2[i]++;
}
firdata2[fir_w_ptr2] = inSampleF;
firptr2[fir_w_ptr2] = 0;
fir_w_ptr2++;
if (fir_w_ptr2 == FILTER_TAP_NUM2) fir_w_ptr2=0;
return (int) outdata;
}
int Calc_FIR3 (int inSample) {
float inSampleF = (float)inSample;
float outdata = 0;
for (int i=0;i < FILTER_TAP_NUM3; i++) {
outdata += (firdata3[i]*filter_taps3[firptr3[i]]);
firptr3[i]++;
}
firdata3[fir_w_ptr3] = inSampleF;
firptr3[fir_w_ptr3] = 0;
fir_w_ptr3++;
if (fir_w_ptr3 == FILTER_TAP_NUM3) fir_w_ptr3=0;
return (int) outdata;
}
int Calc_FIR4 (int inSample) {
float inSampleF = (float)inSample;
float outdata = 0;
for (int i=0;i < FILTER_TAP_NUM4; i++) {
outdata += (firdata4[i]*filter_taps4[firptr4[i]]);
firptr4[i]++;
}
firdata4[fir_w_ptr4] = inSampleF;
firptr4[fir_w_ptr4] = 0;
fir_w_ptr4++;
if (fir_w_ptr4 == FILTER_TAP_NUM4) fir_w_ptr4=0;
return (int) outdata;
}
int Calc_FIR5 (int inSample) {
float inSampleF = (float)inSample;
float outdata = 0;
for (int i=0;i < FILTER_TAP_NUM5; i++) {
outdata += (firdata5[i]*filter_taps5[firptr5[i]]);
firptr5[i]++;
}
firdata5[fir_w_ptr5] = inSampleF;
firptr5[fir_w_ptr5] = 0;
fir_w_ptr5++;
if (fir_w_ptr5 == FILTER_TAP_NUM5) fir_w_ptr5=0;
return (int) outdata;
}
int Calc_FIR6 (int inSample) {
float inSampleF = (float)inSample;
float outdata = 0;
for (int i=0;i < FILTER_TAP_NUM6; i++) {
outdata += (firdata6[i]*filter_taps6[firptr6[i]]);
firptr6[i]++;
}
firdata6[fir_w_ptr6] = inSampleF;
firptr6[fir_w_ptr6] = 0;
fir_w_ptr6++;
if (fir_w_ptr6 == FILTER_TAP_NUM6) fir_w_ptr6=0;
return (int) outdata;
}
/*
int Calc_FIR7 (int inSample) {
float inSampleF = (float)inSample;
float outdata = 0;
for (int i=0;i < FILTER_TAP_NUM7; i++) {
outdata += (firdata7[i]*filter_taps7[firptr7[i]]);
firptr7[i]++;
}
firdata7[fir_w_ptr7] = inSampleF;
firptr7[fir_w_ptr7] = 0;
fir_w_ptr7++;
if (fir_w_ptr7 == FILTER_TAP_NUM7) fir_w_ptr7=0;
return (int) outdata;
}
int Calc_FIR8 (int inSample) {
float inSampleF = (float)inSample;
float outdata = 0;
for (int i=0;i < FILTER_TAP_NUM8; i++) {
outdata += (firdata8[i]*filter_taps8[firptr8[i]]);
firptr8[i]++;
}
firdata8[fir_w_ptr8] = inSampleF;
firptr8[fir_w_ptr8] = 0;
fir_w_ptr8++;
if (fir_w_ptr8 == FILTER_TAP_NUM8) fir_w_ptr8=0;
return (int) outdata;
}
*/
int Calc_FIR9 (int inSample) {
float inSampleF = (float)inSample;
float outdata = 0;
for (int i=0;i < FILTER_TAP_NUM9; i++) {
outdata += (firdata9[i]*filter_taps9[firptr9[i]]);
firptr9[i]++;
}
firdata9[fir_w_ptr9] = inSampleF;
firptr9[fir_w_ptr9] = 0;
fir_w_ptr9++;
if (fir_w_ptr9 == FILTER_TAP_NUM9) fir_w_ptr9=0;
return (int) outdata;
}
int Calc_FIR10 (int inSample) {
float inSampleF = (float)inSample;
float outdata = 0;
for (int i=0;i < FILTER_TAP_NUM10; i++) {
outdata += (firdata10[i]*filter_taps10[firptr10[i]]);
firptr10[i]++;
}
firdata10[fir_w_ptr10] = inSampleF;
firptr10[fir_w_ptr10] = 0;
fir_w_ptr10++;
if (fir_w_ptr10 == FILTER_TAP_NUM10) fir_w_ptr10=0;
return (int) outdata;
}
int Calc_FIR11 (int inSample) {
float inSampleF = (float)inSample;
float outdata = 0;
for (int i=0;i < FILTER_TAP_NUM11; i++) {
outdata += (firdata11[i]*filter_taps11[firptr11[i]]);
firptr11[i]++;
}
firdata11[fir_w_ptr11] = inSampleF;
firptr11[fir_w_ptr11] = 0;
fir_w_ptr11++;
if (fir_w_ptr11 == FILTER_TAP_NUM11) fir_w_ptr11=0;
return (int) outdata;
}
int Calc_FIR12 (int inSample) {
float inSampleF = (float)inSample;
float outdata = 0;
for (int i=0;i < FILTER_TAP_NUM12; i++) {
outdata += (firdata12[i]*filter_taps12[firptr12[i]]);
firptr12[i]++;
}
firdata12[fir_w_ptr12] = inSampleF;
firptr12[fir_w_ptr12] = 0;
fir_w_ptr12++;
if (fir_w_ptr12 == FILTER_TAP_NUM12) fir_w_ptr12=0;
return (int) outdata;
}
int Calc_FIR13 (int inSample) {
float inSampleF = (float)inSample;
float outdata = 0;
for (int i=0;i < FILTER_TAP_NUM13; i++) {
outdata += (firdata13[i]*filter_taps13[firptr13[i]]);
firptr13[i]++;
}
firdata13[fir_w_ptr13] = inSampleF;
firptr13[fir_w_ptr13] = 0;
fir_w_ptr13++;
if (fir_w_ptr13 == FILTER_TAP_NUM13) fir_w_ptr13=0;
return (int) outdata;
}
int Calc_FIR14 (int inSample) {
float inSampleF = (float)inSample;
float outdata = 0;
for (int i=0;i < FILTER_TAP_NUM14; i++) {
outdata += (firdata14[i]*filter_taps14[firptr14[i]]);
firptr14[i]++;
}
firdata14[fir_w_ptr14] = inSampleF;
firptr14[fir_w_ptr14] = 0;
fir_w_ptr14++;
if (fir_w_ptr14 == FILTER_TAP_NUM14) fir_w_ptr14=0;
return (int) outdata;
}
int Calc_FIR15 (int inSample) {
float inSampleF = (float)inSample;
float outdata = 0;
for (int i=0;i < FILTER_TAP_NUM15; i++) {
outdata += (firdata15[i]*filter_taps15[firptr15[i]]);
firptr15[i]++;
}
firdata15[fir_w_ptr15] = inSampleF;
firptr15[fir_w_ptr15] = 0;
fir_w_ptr15++;
if (fir_w_ptr15 == FILTER_TAP_NUM15) fir_w_ptr15=0;
return (int) outdata;
}
int Calc_FIR16 (int inSample) {
float inSampleF = (float)inSample;
float outdata = 0;
for (int i=0;i < FILTER_TAP_NUM16; i++) {
outdata += (firdata16[i]*filter_taps16[firptr16[i]]);
firptr16[i]++;
}
firdata16[fir_w_ptr16] = inSampleF;
firptr16[fir_w_ptr16] = 0;
fir_w_ptr16++;
if (fir_w_ptr16 == FILTER_TAP_NUM16) fir_w_ptr16=0;
return (int) outdata;
}
int Calc_IIR_Left (int inSample) {
float inSampleF = (float)inSample;
float outSampleF =
l_a0 * inSampleF
+ l_a1 * lin_z1
+ l_a2 * lin_z2
- l_b1 * lout_z1
- l_b2 * lout_z2;
lin_z2 = lin_z1;
lin_z1 = inSampleF;
lout_z2 = lout_z1;
lout_z1 = outSampleF;
return (int) outSampleF;
}
int Calc_IIR_Right (int inSample) {
float inSampleF = (float)inSample;
float outSampleF =
r_a0 * inSampleF
+ r_a1 * rin_z1
+ r_a2 * rin_z2
- r_b1 * rout_z1
- r_b2 * rout_z2;
rin_z2 = rin_z1;
rin_z1 = inSampleF;
rout_z2 = rout_z1;
rout_z1 = outSampleF;
return (int) outSampleF;
}
void HAL_I2SEx_TxRxHalfCpltCallback(I2S_HandleTypeDef *hi2s){
//restore signed 24 bit sample from 16-bit buffers
int lSample = (int) (rxBuf[0]<<16)|rxBuf[1];
int rSample = (int) (rxBuf[2]<<16)|rxBuf[3];
// divide by 2 (rightshift) -> -6dB per sample
lSample = lSample>>1;
rSample = rSample>>1;
//sum to mono
lSample = rSample + lSample;
/*
//run HP on left channel and LP on right channel
lSample = Calc_FIR(lSample);
*/
if(mode == 0)
lSample = Calc_FIR1(lSample);
if(mode == 1)
lSample = Calc_FIR2(lSample);
if(mode == 2)
lSample = Calc_FIR3(lSample);
if(mode == 3)
lSample = Calc_FIR4(lSample);
if(mode == 4)
lSample = Calc_FIR5(lSample);
if(mode == 5)
lSample = Calc_FIR6(lSample);
if(mode == 6)
lSample = Calc_IIR_Left(lSample);
if(mode == 7)
lSample = Calc_IIR_Right(lSample);
if(mode == 8)
lSample = Calc_FIR9(lSample);
if(mode == 9)
lSample = Calc_FIR10(lSample);
if(mode == 10)
lSample = Calc_FIR11(lSample);
if(mode == 11)
lSample = Calc_FIR12(lSample);
if(mode == 12)
lSample = Calc_FIR13(lSample);
if(mode == 13)
lSample = Calc_FIR14(lSample);
if(mode == 14)
lSample = Calc_FIR15(lSample);
if(mode == 15)
lSample = Calc_FIR16(lSample);
//restore to buffer
txBuf[0] = (lSample>>16)&0xFFFF;
txBuf[1] = lSample&0xFFFF;
txBuf[2] = (lSample>>16)&0xFFFF;
txBuf[3] = lSample&0xFFFF;
}
void HAL_I2SEx_TxRxCpltCallback(I2S_HandleTypeDef *hi2s){
//restore signed 24 bit sample from 16-bit buffers
int lSample = (int) (rxBuf[4]<<16)|rxBuf[5];
int rSample = (int) (rxBuf[6]<<16)|rxBuf[7];
// divide by 2 (rightshift) -> -6dB per sample
lSample = lSample>>1;
rSample = rSample>>1;
//sum to mono
lSample = rSample + lSample;
/*
//run HP on left channel and LP on right channel
lSample = Calc_FIR(lSample);
*/
if(mode == 0)
lSample = Calc_FIR1(lSample);
if(mode == 1)
lSample = Calc_FIR2(lSample);
if(mode == 2)
lSample = Calc_FIR3(lSample);
if(mode == 3)
lSample = Calc_FIR4(lSample);
if(mode == 4)
lSample = Calc_FIR5(lSample);
if(mode == 5)
lSample = Calc_FIR6(lSample);
if(mode == 6)
lSample = Calc_IIR_Left(lSample);
if(mode == 7)
lSample = Calc_IIR_Right(lSample);
if(mode == 8)
lSample = Calc_FIR9(lSample);
if(mode == 9)
lSample = Calc_FIR10(lSample);
if(mode == 10)
lSample = Calc_FIR11(lSample);
if(mode == 11)
lSample = Calc_FIR12(lSample);
if(mode == 12)
lSample = Calc_FIR13(lSample);
if(mode == 13)
lSample = Calc_FIR14(lSample);
if(mode == 14)
lSample = Calc_FIR15(lSample);
if(mode == 15)
lSample = Calc_FIR16(lSample);
//restore to buffer
txBuf[4] = (lSample>>16)&0xFFFF;
txBuf[5] = lSample&0xFFFF;
txBuf[6] = (lSample>>16)&0xFFFF;
txBuf[7] = lSample&0xFFFF;
}
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0};
/** Configure the main internal regulator output voltage
*/
__HAL_RCC_PWR_CLK_ENABLE();
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
/** Initializes the CPU, AHB and APB busses clocks
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
RCC_OscInitStruct.HSEState = RCC_HSE_ON;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
RCC_OscInitStruct.PLL.PLLM = 8;
RCC_OscInitStruct.PLL.PLLN = 336;
RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
RCC_OscInitStruct.PLL.PLLQ = 7;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB busses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_5) != HAL_OK)
{
Error_Handler();
}
PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_I2S;
PeriphClkInitStruct.PLLI2S.PLLI2SN = 192;//96 kHz 192 -2,34% 197+0,23% 196-0,36%
PeriphClkInitStruct.PLLI2S.PLLI2SR = 2;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
{
Error_Handler();
}
}
/**
* @brief I2S2 Initialization Function
* @PAram None
* @retval None
*/
static void MX_I2S2_Init(void)
{
/* USER CODE BEGIN I2S2_Init 0 */
/* USER CODE END I2S2_Init 0 */
/* USER CODE BEGIN I2S2_Init 1 */
/* USER CODE END I2S2_Init 1 */
hi2s2.Instance = SPI2;
hi2s2.Init.Mode = I2S_MODE_MASTER_TX;
hi2s2.Init.Standard = I2S_STANDARD_PHILIPS;
hi2s2.Init.DataFormat = I2S_DATAFORMAT_24B;
hi2s2.Init.MCLKOutput = I2S_MCLKOUTPUT_ENABLE;
hi2s2.Init.AudioFreq = I2S_AUDIOFREQ_48K;
hi2s2.Init.CPOL = I2S_CPOL_LOW;
hi2s2.Init.ClockSource = I2S_CLOCK_PLL;
hi2s2.Init.FullDuplexMode = I2S_FULLDUPLEXMODE_ENABLE;
if (HAL_I2S_Init(&hi2s2) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN I2S2_Init 2 */
/* USER CODE END I2S2_Init 2 */
}
/**
* Enable DMA controller clock
*/
static void MX_DMA_Init(void)
{
/* DMA controller clock enable */
__HAL_RCC_DMA1_CLK_ENABLE();
/* DMA interrupt init */
/* DMA1_Stream3_IRQn interrupt configuration */
HAL_NVIC_SetPriority(DMA1_Stream3_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(DMA1_Stream3_IRQn);
/* DMA1_Stream4_IRQn interrupt configuration */
HAL_NVIC_SetPriority(DMA1_Stream4_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(DMA1_Stream4_IRQn);
}
/**
* @brief GPIO Initialization Function
* @PAram None
* @retval None
*/
static void MX_GPIO_Init(void)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
/* GPIO Ports Clock Enable */
__HAL_RCC_GPIOE_CLK_ENABLE();
__HAL_RCC_GPIOC_CLK_ENABLE();
__HAL_RCC_GPIOH_CLK_ENABLE();
__HAL_RCC_GPIOA_CLK_ENABLE();
__HAL_RCC_GPIOB_CLK_ENABLE();
__HAL_RCC_GPIOD_CLK_ENABLE();
/*Configure GPIO pin Output Level */
HAL_GPIO_WritePin(GPIOE, GPIO_PIN_3, GPIO_PIN_RESET);
/*Configure GPIO pin Output Level */
HAL_GPIO_WritePin(GPIOC, GPIO_PIN_0, GPIO_PIN_RESET);
/*Configure GPIO pin Output Level */
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12|GPIO_PIN_13|GPIO_PIN_14|GPIO_PIN_15
|GPIO_PIN_4, GPIO_PIN_RESET);
/*Configure GPIO pin : PE3 */
GPIO_InitStruct.Pin = GPIO_PIN_3;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(GPIOE, &GPIO_InitStruct);
/*Configure GPIO pin : PC0 */
GPIO_InitStruct.Pin = GPIO_PIN_0;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
/*Configure GPIO pin : PA0 */
GPIO_InitStruct.Pin = GPIO_PIN_0;
GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING;
GPIO_InitStruct.Pull = GPIO_NOPULL;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
/*Configure GPIO pin : PA4 */
GPIO_InitStruct.Pin = GPIO_PIN_4;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
GPIO_InitStruct.Alternate = GPIO_AF6_SPI3;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
/*Configure GPIO pins : PA5 PA6 PA7 */
GPIO_InitStruct.Pin = GPIO_PIN_5|GPIO_PIN_6|GPIO_PIN_7;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF5_SPI1;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
/*Configure GPIO pin : PB2 */
GPIO_InitStruct.Pin = GPIO_PIN_2;
GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
GPIO_InitStruct.Pull = GPIO_NOPULL;
HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
/*Configure GPIO pins : PD12 PD13 PD14 PD15
PD4 */
GPIO_InitStruct.Pin = GPIO_PIN_12|GPIO_PIN_13|GPIO_PIN_14|GPIO_PIN_15
|GPIO_PIN_4;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(GPIOD, &GPIO_InitStruct);
/*Configure GPIO pins : PC7 PC10 PC12 */
GPIO_InitStruct.Pin = GPIO_PIN_7|GPIO_PIN_10|GPIO_PIN_12;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
GPIO_InitStruct.Alternate = GPIO_AF6_SPI3;
HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
/*Configure GPIO pin : PA9 */
GPIO_InitStruct.Pin = GPIO_PIN_9;
GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
GPIO_InitStruct.Pull = GPIO_NOPULL;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
/*Configure GPIO pins : PA10 PA11 PA12 */
GPIO_InitStruct.Pin = GPIO_PIN_10|GPIO_PIN_11|GPIO_PIN_12;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF10_OTG_FS;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
/*Configure GPIO pin : PD5 */
GPIO_InitStruct.Pin = GPIO_PIN_5;
GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
GPIO_InitStruct.Pull = GPIO_NOPULL;
HAL_GPIO_Init(GPIOD, &GPIO_InitStruct);
/*Configure GPIO pins : PB6 PB9 */
GPIO_InitStruct.Pin = GPIO_PIN_6|GPIO_PIN_9;
GPIO_InitStruct.Mode = GPIO_MODE_AF_OD;
GPIO_InitStruct.Pull = GPIO_PULLUP;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF4_I2C1;
HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
/*Configure GPIO pin : PE1 */
GPIO_InitStruct.Pin = GPIO_PIN_1;
GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING;
GPIO_InitStruct.Pull = GPIO_NOPULL;
HAL_GPIO_Init(GPIOE, &GPIO_InitStruct);
/* EXTI interrupt init*/
HAL_NVIC_SetPriority(EXTI0_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(EXTI0_IRQn);
}
// @brief RNG Initialization Function
static void MX_RNG_Init(void)
{
/* USER CODE BEGIN RNG_Init 0 */
/* USER CODE END RNG_Init 0 */
/* USER CODE BEGIN RNG_Init 1 */
/* USER CODE END RNG_Init 1 */
hrng.Instance = RNG;
if (HAL_RNG_Init(&hrng) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN RNG_Init 2 */
/* USER CODE END RNG_Init 2 */
}
void HAL_RNG_MspInit(RNG_HandleTypeDef* hrng)
{
if(hrng->Instance==RNG)
{
/* USER CODE BEGIN RNG_MspInit 0 */
/* USER CODE END RNG_MspInit 0 */
/* Peripheral clock enable */
__HAL_RCC_RNG_CLK_ENABLE();
/* USER CODE BEGIN RNG_MspInit 1 */
/* USER CODE END RNG_MspInit 1 */
}
}
/**
* @brief RNG MSP De-Initialization
* This function freeze the hardware resources used in this example
* @PAram hrng: RNG handle pointer
* @retval None
*/
void HAL_RNG_MspDeInit(RNG_HandleTypeDef* hrng)
{
if(hrng->Instance==RNG)
{
/* USER CODE BEGIN RNG_MspDeInit 0 */
/* USER CODE END RNG_MspDeInit 0 */
/* Peripheral clock disable */
__HAL_RCC_RNG_CLK_DISABLE();
/* USER CODE BEGIN RNG_MspDeInit 1 */
/* USER CODE END RNG_MspDeInit 1 */
}
}
void Error_Handler(void)
{
/* USER CODE BEGIN Error_Handler_Debug */
/* User can add his own implementation to report the HAL error return state */
/* USER CODE END Error_Handler_Debug */
}
#ifdef USE_FULL_ASSERT
/**
* @brief Reports the name of the source file and the source line number
* where the assert_param error has occurred.
* @PAram file: pointer to the source file name
* @PAram line: assert_param error line source number
* @retval None
*/
void assert_failed(uint8_t *file, uint32_t line)
{
/* USER CODE BEGIN 6 */
/* User can add his own implementation to report the file name and line number,
tex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
/* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */
/************************ (C) COPYRIGHT STMicroelectronics *****END OF FILE****/