STMG474RE USB FS implementation
Hi together,
i´m trying to set up a communication via usb using the usb cdc class to communicate with additional software via a virtual com port running on a local pc using the Nucleo G474RE board.
However i can't find a sufficient documentation what i do have to implement / settings that have to be done to send and recieve data.
I`ve also watched the youtube tutorial from stm on the topic usb cdc but it didn't help me.
I made the following steps until now in the cube ide:
I´ve activated the usb in the communication section and the usb_device in the middleware where i also set the communication device class option.


Afterwards i solved the clock issue using the HSI48RC clock for usb.

But from that on the next steps are unclear to me. Can i now just use the "uint8_t CDC_Transmit_FS(uint8_t* Buf, uint16_t Len)" function to transmit data? This function is located in the usbd_cdc_if.h/c file.


I tried a short example using this function to send a short hello world char array but it didn't work. So i think i missed something.
I searched in the reference manual, the datasheet and the HAL documentation for any hints but i couldn't find any - have i overlooked something?
Especially for the USB functions i couldn't find any description except in the corresponding h/c files.
I hope this description is sufficient. Thank`s for your help.