Skip to main content
Visitor II
August 29, 2024
Question

STMicroelectronics ST-LINK GDB server. Version 7.5.0 Copyri

  • August 29, 2024
  • 1 reply
  • 663 views

libusb: info [darwin_claim_interface] no interface found; setting configuration: 1

 

Device : MACBOOK AIR

 

STMicroelectronics ST-LINK GDB server. Version 7.5.0

Copyright (c) 2023, STMicroelectronics. All rights reserved.

 

Starting server with the following options:

Persistent Mode : Disabled

Logging Level : 1

Listen Port Number : 61234

Status Refresh Delay : 15s

Verbose Mode : Disabled

SWD Debug : Enabled

InitWhile : Enabled

 

libusb: error [darwin_claim_interface] could not set configuration

Device connect error

 

Error in initializing ST-LINK device.

Reason: Failed to connect to device. Please check power and cabling to target.

@Developer_1 

    This topic has been closed for replies.

    1 reply

    Super User
    August 30, 2024

    Try to connect the ST-LINK thru a hub (better a powered one).