Strange Behaviour HAL_TIM_PWM_Start_DMA
Hello everyone.
I am encountering a very strange issue with the STM32H7B0 using the J-Link to debug.
I followed this tutorial to control the WS28B12 LED using Timer, PWM and DMA.
I use the following function to transmit the PWM data.
if (HAL_TIM_PWM_Start_DMA(&htim1, TIM_CHANNEL_1, address, 74) != HAL_OK) Error_Handler();But here comes the strange thing:
If i run the code, nothing happens, or lets say, the data doesn't get transmitted:

But if i look at value of the address variable in the debugger before running the ...Start_DMA...:

And then Resume the program it suddenly works:

Why does this happen?
Any help is appreciated