Strange variable behavior in struct, TCP / lwIP
Heyho,
I have a super-stable TCP-audio-streaming server on a H733 here, using custom ETH driver and lwIP, no OS.
But I recently found that in a struct which is used for handling / storing the TCP connection, the variable to store the port number "u16Port" (used in lwIP's tcp_bind() to set the TCP port) changes as soon as data is transmitted.
It's really crazy: u16Port has the init value before and after the connection is accepted, but as soon as data is transmitted, it changes all the time (checked via UART and http REST). When data transfer stops, it keeps the latest wrong value, after TCP connection is closed, u16Port has the init value again.
All other values in the struct do NOT change and their values make sense.
I have tried to set the struct to volatile, use another memory area, align, but still changing.
I just checked it with the STM32CubeIDE debugger under Live Expressions, there I see the same change.
I admit I have no idea how I can check where this variable is modified.
How can I find out where the variable is modified?
Any ideas what's happening?
/* ++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++ */
/* struct for handling TCP
* CONTROL
*/
struct s_sTcpStreamControl
{
struct tcp_pcb *pPcbListen;
struct tcp_pcb *pPcbStream;
uint16_t u16Port;
uint16_t u16Dummy;
sTcpStreamConnection_t *psCon;
sTcpStreamCounters_t sCnt;
uint32_t u32RxdBytes;
uint8_t u8CtlState;
uint8_t u8SrvActive;
uint8_t u8SrvStop;
uint8_t u8SrvAcptStartPeriph;
};
typedef struct s_sTcpStreamControl sTcpStreamControl_t;
...
/* A2IP = audio to IP control */
sTcpStreamControl_t sTcpStreamCtrlA2Ip;