Skip to main content
Visitor II
March 11, 2024
Solved

STSW-IO-LINK on STEVAL-IDP004V2

  • March 11, 2024
  • 1 reply
  • 2648 views

How to open the STSW-IO-LINK evaluation firmware in the STM32CubeMX development platform? STSW-IO-Link is downloaded and extracted. The *.ioc file seems to be missing in the STSW-IO-LINK firmware package!

    This topic has been closed for replies.
    Best answer by STTwo-32

    1. STSW-IO-LINK firmware is developed using IAR.

    2. take a look at this video.

    Best regards.

    STTwo-32

     

    1 reply

    Technical Moderator
    March 11, 2024

    Hello @Luna and welcome to the ST Community :smiling_face_with_smiling_eyes:.

    The examples of this firmware are not developed starting from CubeMX configurations. So, there is not a .ioc file on the projects.

    Best regards.

    STTwo-32 

    LunaAuthor
    Visitor II
    March 12, 2024

    thanks for your information. if I want to change the firmware code and download it to MCU, do i need to start from 0 to create my own project and code? or do I have any other ways more easier?

    Technical Moderator
    March 12, 2024

    Changes should be done directly on the code or by starting a new project.

    Best Regards.

    STTwo-32