Skip to main content
Visitor II
September 4, 2024
Question

STSW-LINK009 Driver Install Fail

  • September 4, 2024
  • 3 replies
  • 1086 views

Hello, 

I am on a MacBook Pro M2 running Parallels Windows 11. 

I have downloaded the STSW-LINK009 zip file. 

Because of my machine, I need to run the dpinst_amd64.exe file. It opens and runs perfectly fine but I am unable to install the drivers as it says "Install Failed" (Provided a screenshot below) 

Driver Install Fail.png

I have disabled the secure boot on Windows 11 to see if it helped, but it did not. 

I'm wondering if it's because these drivers are not compatible with my Mac M2, or if I need to take another route.

Any help will be amazing. Thank you. 

    This topic has been closed for replies.

    3 replies

    Visitor II
    September 14, 2024

    Experiencing the same problem in my Microsoft Surface Pro 11 (ARM) laptop. Would highly appreciate a solution.

     

    Graduate
    September 15, 2024

    Why are you using win11?

    Visitor II
    November 19, 2024

    Experiencing the same. And without these drivers I am getting "No debug probe detected" :weary_face: