Stuck USB peripheral does not recover after a NRST...needs power cycle...
Hi STM32 community.
I'm working on an embedded system which uses a RK3399 CPU (running Linux, functions as a USB host) and a STM32F302CC (Runing FreeRTOS, functions as a USB device). This runs on a custom motherboard. They communicate with each other through virtual COM ports over USB (using this library https://github.com/IntergatedCircuits/USBDevice).
This embedded system has been around and in use for several years and thousands of units are operational. 99,99% of the time (or something like that) everything just works just perfectly. But every now and then, during some special circumstances which have not yet been fully understood (MCU brownout maybe?), some devices will end up in a weird state where the MCU seems to be running, but the USB device (i.e. the STM32F302CC) does not enumerate in Linux on the CPU side. This can be seen in kernel log as something like this (or similar):
[81228.001719] usb 7-1.4: new full-speed USB device number 40 using xhci-hcd
[81228.065694] usb 7-1.4: device descriptor read/64, error -32
[81228.244730] usb 7-1.4: device descriptor read/64, error -32
[81228.420638] usb 7-1.4: new full-speed USB device number 41 using xhci-hcd
[81228.484767] usb 7-1.4: device descriptor read/64, error -32
[81228.660677] usb 7-1.4: device descriptor read/64, error -32
[81228.772925] usb 7-1-port4: attempt power cycle
[81229.352634] usb 7-1.4: new full-speed USB device number 42 using xhci-hcd
[81229.352740] usb 7-1.4: Device not responding to setup address.
[81229.556702] usb 7-1.4: Device not responding to setup address.
[81229.764596] usb 7-1.4: device not accepting address 42, error -71
[81229.835597] usb 7-1.4: new full-speed USB device number 43 using xhci-hcd
[81229.835696] usb 7-1.4: Device not responding to setup address.
[81230.044687] usb 7-1.4: Device not responding to setup address.
[81230.252587] usb 7-1.4: device not accepting address 43, error -71
[81230.260076] usb 7-1-port4: unable to enumerate USB device
User-space code in Linux will notice that the expected serial port (a virtual COM port over USB) never appears and will eventually perform a NRST reset on the MCU using CPU GPIO pins connected to MCU NRST pin. The CPU will perform another reset if needed, over and over (there are a several seconds wait time in between the resets of course) until the COM port shows up, which it never does in this case. These resets definitely do happen in the MCU (can be confirmed for example by following the debug UART from the MCU or by looking with oscilloscope on the NRST line). However, the MCU reset does not fix the USB enumeration issue. USB will still not enumerate in Linux after the MCU have been reset. And doing the same reset manually by shorting the MCU NRST pin directly on the circuit board also does not help to recover the USB numeration issue. Rebooting the CPU also does not help. Power cycling the CPU does not help either. But physically cutting the power completely from the MCU (POR/PDR reset) does indeed help, every single time. After a POR/PDR reset everything works again, every single time.
One would assume that a NRST reset would be enough for a stuck USB peripheral to fully recover, but it seems not to be the case. I cannot find anything about this in STM32F302xB/C Errata sheet (ES0231 Rev 6).
This is what the RM0365 Reference manual says about resets
9.1.1 Power reset
A power reset is generated when one of the following events occurs:
1. Power-on/power-down reset (POR/PDR reset)
2. When exiting Standby mode
A power reset sets all registers to their reset values except the RTC domain (see Figure 8).
9.1.2 System reset
A system reset sets all registers to their reset values except the reset flags in the clock
controller CSR register and the registers in the RTC domain (see Figure 8).
A system reset is generated when one of the following events occurs:
1. A low level on the NRST pin (external reset)
2. Window watchdog event (WWDG reset)
3. Independent watchdog event (IWDG reset)
4. A software reset (SW reset) (see Software reset)
5. Low-power management reset (see Low-power management reset)
6. Option byte loader reset (see Option byte loader reset)
7. A power reset
The reset source can be identified by checking the reset flags in the Control/Status register,
RCC_CSR (see Section 9.4.10: Control/status register (RCC_CSR)).
These sources act on the NRST pin and it is always kept low during the delay phase. The
RESET service routine vector is fixed at address 0x0000_0004 in the memory map.
The system reset signal provided to the device is output on the NRST pin. The pulse
generator guarantees a minimum reset pulse duration of 20 μs for each internal reset
source. In case of an external reset, the reset pulse is generated while the NRST pin is
asserted low.
The initialization order of the USB peripheral is already done as described in the technical reference manual, and I have discussed with ChatGPT about possible improvements. But everything it has suggested either just breaks the USB enumeration completely or even worse, causes the whole MCU to hang. And anyway, the current code works 99,99% of the time and has done so for several years, so it must be somewhat correct.
So what I'm mainly wondering is if there is any known issues when the USB peripheral inside the STM32F302CC can end up in such a bad state the only a power cycle will reset it properly? If so, could anyone elaborate on what might cause this (brownout during USB operation etc.) so that if I cannot recover from it at least I can try to minimize the risk of it ending up in this state to begin with.
Currently the CPU can not cut the power from the MCU (but I can do it by hand on the circuit board), so "fixing" it that way would require a new HW revision. And anyway would not help in the many devices already in circulation.
Any relevant input which even remotely could be related to what I'm seeing is appreciated!