Synchronize peripherals SAI & I2S output clocks
Heyho,
I'm using a H733 with both SAI 1 and SAI 4 with SAI 1 as I2S clock master to get 8 synced audio channels.
Audio clock comes from I2SCKIN, this is used for SAIs and I2S.
Problem: because of the fixed oversampling ratio (256 or 512) of the SAI, I have to use an SPI/I2S peripheral to generate the "MCLK" to make 200 kHz possible, with 200 kHz x 128 = 25.6 MHz.
That's basically working, but I wonder why sometimes at start (not while running) the MCLK (from SPI/I2S) shifts by 180° / is inverted, in relation to the SAI/I2S clocks (SCLK (=SCK), LRCK (=WS)).
For regular audio stuff this is not a problem, but I have another slave on the I2S bus doing other things which needs a fixed phase relation between MCLK and LRCK / SCLK (previously controlled by an FPGA).
So how are theses clocks generated that this phase shift can happen, with the same clock input , and "going through" the same hardware each time?
What can I do to sync these clocks?