SysTick and clock configuration
Hi to all,
I have a problem with clock and systick configuration.
I am using an STM32F303CBT MCU and STMCubeIDE.
At present my program realize a blinking led, but if I do not activate SysTick after a randon mumber of blinking the led stuck on or off indefinitely.
If I try to activate systick, the SysTick_Handler() works five times and then it stucks.
Here is my code:
void SystemInit()
{
/* Clock init */
/*-------------------------------- HSI Configuration -----------------------*/
if((RCC->CFGR & RCC_CFGR_SWS_Msk) != RCC_CFGR_SWS_HSI) // If HSI is not used as SystemClock
{
RCC->CFGR &= ~RCC_CFGR_SW_Msk; // Select HSI as SystemClock
RCC->CFGR |= RCC_CFGR_SW_HSI;
while((RCC->CFGR & RCC_CFGR_SWS_Msk) != RCC_CFGR_SWS_HSI); // Wait for HSI ready
}
if(RCC->CR & RCC_CR_PLLON) RCC->CR &= ~RCC_CR_PLLON; //Disable PLL
// while(RCC->CR & RCC_CR_PLLRDY); // Wait for PLL disabled
RCC->CFGR &= ~(RCC_CFGR_MCO_Msk | RCC_CFGR_USBPRE_Msk | RCC_CFGR_PLLMUL_Msk | RCC_CFGR_PLLSRC_Msk | RCC_CFGR_PPRE2_Msk | RCC_CFGR_PPRE1_Msk | RCC_CFGR_HPRE_Msk | RCC_CFGR_SW_Msk); //Clear register's bits
RCC->CFGR |= RCC_CFGR_MCO_HSI | RCC_CFGR_USBPRE_DIV1 | RCC_CFGR_PLLMUL12 | RCC_CFGR_PLLSRC_HSI_DIV2 | RCC_CFGR_PPRE2_DIV1 | RCC_CFGR_PPRE1_DIV2 | RCC_CFGR_HPRE_DIV1 | RCC_CFGR_SW_PLL;
RCC->CR |= RCC_CR_PLLON; //PLLON
while(!(RCC->CR & RCC_CR_PLLRDY)); // Wait for PLL enabled
if(!(RCC->CFGR & RCC_CFGR_SWS_PLL))
{
RCC->CFGR &= ~RCC_CFGR_SW_Msk;
RCC->CFGR |= RCC_CFGR_SW_PLL; // if PLL is not SystemClock, set PLL as SystemClock
}
mysysclock = 48000; // in MHz
RCC->CIR = 0x009F0000;
return;
}
int main(void)
{
uint32_t ccc=0;
myled.LedOff(LED0);
/* SysTick end of count event each 0,1 sec */
SysTick->CTRL |= SYSTICK_CLKSOURCE_HCLK;
SysTick_Config(100*mysysclock);
while(1)
{
ccc++;
}
}
extern "C" void SysTick_Handler()
{
myled.Toggle(LED0);
return;
}
I compared it with a similar one generated with CubeMX and I think I did forgot nothing (but probally I failed)
Where can I check where i the problem?
Thank you
Freya