task doesn't start when run in ram
hello:
I use NUCLEO-H7A3ZI-Q to test a bootloader feature:the bootloader runs in 0x08000000 at flash, when it starts, it copies the application stored in 0x08005000 to 0x24000000 in RAM, then jump to 0x24000000, I turn on a led in main function to signal the success, so far it works well, but if I put the turn on code in a task, the led won't be turned on, which means the task fails to run, also if I use HAL_Delay in main, it will be stuck in HAL_Delay, can anyone help me out? Thanks.
Bill