TCA9539 use as a GPIO Port Expander with STM32F091RCT6
Hello.
I would like touse TCA9539 use as a GPIO Port Expander with STM32F091RCT6 (IO-EXPANDER-EVM Evaluation board | TI.com). I have enabled I2C2 in STM and connect as follows
STM32F091RCT6
SCL------------------------>I2C2_SCL PB10
SDA------------------------>I2C2_SDA PB11
VCC------------------------>5V
GND------------------------>GND
And below the generated code
#include "main.h"
#include "i2c.h"
#include "usart.h"
#include "gpio.h"
#include "stm32f0xx_hal.h"
#define TCA9539_ADDR 0x74 << 1
#define INPUT_PORT0_REG 0x00
#define OUTPUT_PORT0_REG 0x02
#define CONFIG_PORT0_REG 0x06
#define INPUT_PORT1_REG 0x01
#define OUTPUT_PORT1_REG 0x03
#define CONFIG_PORT1_REG 0x07
void SystemClock_Config(void);
void TCA9539_Init(void) {
uint8_t data[3];
data[0] = CONFIG_PORT0_REG;
data[1] = 0x00; // 0x00 for output
HAL_I2C_Master_Transmit(&hi2c2, TCA9539_ADDR, data, 2, HAL_MAX_DELAY);
data[0] = CONFIG_PORT1_REG;
data[1] = 0x00; // 0x00 for output
HAL_I2C_Master_Transmit(&hi2c2, TCA9539_ADDR, data, 2, HAL_MAX_DELAY);
}
void Control_LEDs(uint8_t port0_state) {
uint8_t data[2];
data[0] = OUTPUT_PORT0_REG;
data[1] = port0_state; // State of each pin: 0 for off, 1 for on
HAL_I2C_Master_Transmit(&hi2c2, TCA9539_ADDR, data, 2, HAL_MAX_DELAY);
}
int main(void)
{
MX_GPIO_Init();
MX_USART2_UART_Init();
MX_I2C2_Init();
MX_USART1_UART_Init();/
TCA9539_Init();
while (1)
{
Control_LEDs(0xFF);
HAL_Delay(1000);
Control_LEDs(0x00);
HAL_Delay(1000);
}
/
}
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
RCC_PeriphCLKInitTypeDef PeriphClkInit = {0};
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
RCC_OscInitStruct.HSIState = RCC_HSI_ON;
RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
RCC_OscInitStruct.PLL.PLLMUL = RCC_PLL_MUL12;
RCC_OscInitStruct.PLL.PREDIV = RCC_PREDIV_DIV2;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_1) != HAL_OK)
{
Error_Handler();
}
PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_USART1|RCC_PERIPHCLK_USART2
|RCC_PERIPHCLK_I2C1;
PeriphClkInit.Usart1ClockSelection = RCC_USART1CLKSOURCE_PCLK1;
PeriphClkInit.Usart2ClockSelection = RCC_USART2CLKSOURCE_PCLK1;
PeriphClkInit.I2c1ClockSelection = RCC_I2C1CLKSOURCE_HSI;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK)
{
Error_Handler();
}
}
void Error_Handler(void)
__disable_irq();
while (1)
{
}
}
#ifdef USE_FULL_ASSERT
void assert_failed(uint8_t *file, uint32_t line)
{
}
#endif /* USE_FULL_ASSERT */
I have tried to turn on and off P00 ~ P07. But its not working.