The 48MHz crystal oscillator for HSE of STM32H743 cannot be realized.
Hello sir/miss ,
According to the STM32H7 datasheet, the range of the HSE external crystal oscillator is 4M - 48MHz. However, when we used the STM32H7IIT6-EVAL evaluation board and replaced the original 25MHz surface mount passive crystal oscillator with a 48MHz passive crystal oscillator, we were unable to obtain the corresponding 48MHz frequency from the MCO-PA8 pin.
Summary: All conventional passive crystals from 4M to 40MHz were tried and worked fine. However, for external passive crystals above 40MHz , just like 48MHz, the MCO output waveform frequency was 16MHz, which is 1/3 of the HSE frequency, and it was unable to output 48MHz.
Please provide a solution or suggest areas where we can improve the test. Thank you very much!