The correct value cannot be read without resetting after flash writing with the B-U585I-IOT02A
I use B-U585I-IOT02A to read after writing Flash Memory, 0xFF is read, but once I reset it, I can read the written value.
Similarly, when I use it to read after erasing the Flash Memory, the value before erasing is read, but once I reset it, I can read 0xFF.
In short, the correct value cannot be read unless reset once for both Write and Erase.
Is there any processing that must be done after programming or erasing?