The microcontroller sometimes cannot receive TCP data
Hi.
In my system, the opposing device sends TCP data at 20ms intervals,
and the microcontroller receives the TCP data non-blocking at 20ms intervals.
Therefore, the ethernetif_input() function of LWIP is supposedto be called at 20ms intervals and store data in the receive buffer.
However, as the operation continues, the calls to ethernetif_input() gradually delay by 1ms, 2ms, and so on.
(After 18 minutes, the calls are delayed by 10ms.)
As a result, there are moments when the receive buffer is empty, causing failures in receiving data at 20ms intervals.
I tried the following, but the call to ethernetif_input() is still gradually delayed:
・Changing the data transmission interval of the counterpart device (20ms → 10ms or 100ms)
・Adjusting the CPU clock (168MHz → 216MHz)
・Changing ETH_RX_DESC_CNT (4 → 8)
・Changing INTERFACE_THREAD_STACK_SIZE (350 → 500)
・Changing TCPIP_MBOX_SIZE (6 → 1000)
・Changing DEFAULT_TCP_RECVMBOX_SIZE (6 → 1000)
How can the microcontroller successfully receive TCP data in every cycle?
Test environment:
Microcontroller : STM32 NUCLEO-F767ZI
Counterpart device : Ubuntu 22.04, ROS2 (C++)
STM32Cube IDE : 1.15.0
STM32 Firmware : STM32_Cube FW_F7 V1.17.1
STM32Cube MX : 6.11.0
LWIP : v2.1.2_Cube
Best regards.