TIM6 Configuration STM32G4
I am having trouble configuring my TIM6 to toggle a GPIO pin every 1 usec. I am using the HSI at 16MHz as the source for AHB bus clocks, which TIM6 is on.
The following is my System Clock configuration:
void SystemClock_Config(void)
{
LL_FLASH_SetLatency(LL_FLASH_LATENCY_0);
while(LL_FLASH_GetLatency() != LL_FLASH_LATENCY_0)
{
}
LL_PWR_SetRegulVoltageScaling(LL_PWR_REGU_VOLTAGE_SCALE1);
LL_RCC_HSI_Enable();
/* Wait till HSI is ready */
while(LL_RCC_HSI_IsReady() != 1)
{
}
LL_RCC_HSI_SetCalibTrimming(64);
LL_RCC_SetSysClkSource(LL_RCC_SYS_CLKSOURCE_HSI);
/* Wait till System clock is ready */
while(LL_RCC_GetSysClkSource() != LL_RCC_SYS_CLKSOURCE_STATUS_HSI)
{
}
/* Set AHB prescaler*/
LL_RCC_SetAHBPrescaler(LL_RCC_SYSCLK_DIV_1);
LL_RCC_SetAPB1Prescaler(LL_RCC_APB1_DIV_1);
LL_RCC_SetAPB2Prescaler(LL_RCC_APB2_DIV_1);
LL_SetSystemCoreClock(16000000);
/* Update the time base */
if (HAL_InitTick (TICK_INT_PRIORITY) != HAL_OK)
{
Error_Handler();
}
}
I am then configuring TIM6 with the following:
static void MX_TIM6_Init(void)
{
/* USER CODE BEGIN TIM6_Init 0 */
/* USER CODE END TIM6_Init 0 */
LL_TIM_InitTypeDef TIM_InitStruct = {0};
/* Peripheral clock enable */
LL_APB1_GRP1_EnableClock(LL_APB1_GRP1_PERIPH_TIM6);
/* TIM6 interrupt Init */
NVIC_SetPriority(TIM6_DAC_IRQn, NVIC_EncodePriority(NVIC_GetPriorityGrouping(),0, 0));
NVIC_EnableIRQ(TIM6_DAC_IRQn);
/* USER CODE BEGIN TIM6_Init 1 */
/* USER CODE END TIM6_Init 1 */
TIM_InitStruct.Prescaler = 16 - 1;
TIM_InitStruct.CounterMode = LL_TIM_COUNTERMODE_UP;
TIM_InitStruct.Autoreload = 1;
LL_TIM_Init(TIM6, &TIM_InitStruct);
LL_TIM_EnableARRPreload(TIM6);
LL_TIM_SetTriggerOutput(TIM6, LL_TIM_TRGO_UPDATE);
LL_TIM_DisableMasterSlaveMode(TIM6);
LL_TIM_EnableIT_UPDATE(TIM6);
/* USER CODE BEGIN TIM6_Init 2 */
/* USER CODE END TIM6_Init 2 */
}
The GPIO is not toggling every usec as I expect it to. Is there something wrong with my configuration?