Timer behaviour after wakeup from STOP
I've searched and not found anything describing this behaviour (on the internet or this forum, which I've found to be an incredible resource so far - thank you).
I have a configuration where I go into STOP, exit out of STOP via EXTI, start TIM1, allow the stack to unwind to leave HAL_PWR_EnterSTOPMode(), and then SLEEP. With this sequence, I expect a TIM1 interrupt but never hear one.
Conversely, if I enter SLEEP instead of STOP for the very first step but perform all of the other steps identically, I get the behaviour I'm looking for - an EXTI, then a period asleep, then a TIM1 callback. This tells me that the STOP is interfering with the configuration of the timer somehow, in a way that I haven't been able to figure out how to recover from.
I've tried, after exiting STOP, to re-issue a call to HAL_TIM_Base_MspInit and MX_TIM1_Init but this has not helped. Removing the final SLEEP and spin-waiting has also not helped.
Why might this be happening? Where should I start the debug effort?