Skip to main content
Visitor II
May 11, 2024
Question

Timer Compare Output using DMA - STM32F3Discovery

  • May 11, 2024
  • 4 replies
  • 3128 views

Hello,

I am attempting to generate a waveform with a period of 33ms. In-between each period, I need to toggle the timer output 5 times with a varying timescale. My initial thought is to do this using a timer in output compare mode and then update the CRR register with the 5 pulses from the DMA in a circular mode.

 ___________ ___________ ___________
 | 5700 |___3000___| 4700 |___3000___| 10000 |_________________________

 <------------------------------------33ms------------------------------------>
 

So far, the pin toggles but at intervals that are over the values in the array. Below is the waveform as seen on a logic analyser. I am certain that the input clock is correct at 36MHz and the period should be 33ms.

daded1_1-1715401969734.png

 

I have included the following functions to the CubeMX generated code to ensure the timer is started with DMA.

HAL_TIM_OC_DelayElapsedCallback(&htim17);
//enable dma
HAL_TIM_OC_Start_DMA(&htim17, TIM_CHANNEL_1, (uint32_t*)wave_buffer, 5);

 At this point, I'm not sure what I'm missing as I've followed the steps in the reference manual and application notes to be on par with what I need. I appreciate any help with what I may be missing, thank you.

PS- code is below

/* USER CODE BEGIN Header */
/**
 ******************************************************************************
 * @file : main.c
 * @brief : Main program body
 ******************************************************************************
**/

/* Private variables ---------------------------------------------------------*/
TIM_HandleTypeDef htim17;
DMA_HandleTypeDef hdma_tim17_ch1_up;

/* USER CODE BEGIN PV */
 uint16_t wave_buffer[5] = {5700, 3000, 4700, 3000, 10000};

/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_DMA_Init(void);
static void MX_TIM17_Init(void);
/* USER CODE BEGIN PFP */

/* USER CODE END PFP */

/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */

/* USER CODE END 0 */

/**
 * @brief The application entry point.
 * @retval int
 */
int main(void)
{

 /* USER CODE BEGIN 1 */

 /*
 ___________ ___________ ___________
 | 5700 |___3000___| 4700 |___3000___| 10000 |_________________________

 <------------------------------------33ms------------------------------------>
 
 */
 /* USER CODE END 1 */

 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();

 /* USER CODE BEGIN Init */

 /* USER CODE END Init */

 /* Configure the system clock */
 SystemClock_Config();

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_DMA_Init();
 MX_TIM17_Init();
 /* USER CODE BEGIN 2 */
 
 // HAL_TIM_OC_DelayElapsedCallback(&htim15);
 HAL_TIM_OC_DelayElapsedCallback(&htim17);
 //enable dma
 HAL_TIM_OC_Start_DMA(&htim17, TIM_CHANNEL_1, (uint32_t*)wave_buffer, 5);

 /* USER CODE END 2 */

 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {
 /* USER CODE END WHILE */

 /* USER CODE BEGIN 3 */
 }
 /* USER CODE END 3 */
}

/**
 * @brief System Clock Configuration
 * @retval None
 */
void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

 /** Initializes the RCC Oscillators according to the specified parameters
 * in the RCC_OscInitTypeDef structure.
 */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
 RCC_OscInitStruct.HSIState = RCC_HSI_ON;
 RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
 RCC_OscInitStruct.PLL.PLLMUL = RCC_PLL_MUL9;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }

 /** Initializes the CPU, AHB and APB buses clocks
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV2;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;

 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_1) != HAL_OK)
 {
 Error_Handler();
 }
}

/**
 * @brief TIM17 Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_TIM17_Init(void)
{

 /* USER CODE BEGIN TIM17_Init 0 */

 /* USER CODE END TIM17_Init 0 */

 TIM_OC_InitTypeDef sConfigOC = {0};
 TIM_BreakDeadTimeConfigTypeDef sBreakDeadTimeConfig = {0};

 /* USER CODE BEGIN TIM17_Init 1 */

 /* USER CODE END TIM17_Init 1 */
 htim17.Instance = TIM17;
 htim17.Init.Prescaler = 36-1;
 htim17.Init.CounterMode = TIM_COUNTERMODE_UP;
 htim17.Init.Period = 33000-1;
 htim17.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
 htim17.Init.RepetitionCounter = 0;
 htim17.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
 if (HAL_TIM_Base_Init(&htim17) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_TIM_OC_Init(&htim17) != HAL_OK)
 {
 Error_Handler();
 }
 sConfigOC.OCMode = TIM_OCMODE_TOGGLE;
 sConfigOC.Pulse = 0;
 sConfigOC.OCPolarity = TIM_OCPOLARITY_LOW;
 sConfigOC.OCNPolarity = TIM_OCNPOLARITY_HIGH;
 sConfigOC.OCFastMode = TIM_OCFAST_DISABLE;
 sConfigOC.OCIdleState = TIM_OCIDLESTATE_RESET;
 sConfigOC.OCNIdleState = TIM_OCNIDLESTATE_RESET;
 if (HAL_TIM_OC_ConfigChannel(&htim17, &sConfigOC, TIM_CHANNEL_1) != HAL_OK)
 {
 Error_Handler();
 }
 __HAL_TIM_ENABLE_OCxPRELOAD(&htim17, TIM_CHANNEL_1);
 sBreakDeadTimeConfig.OffStateRunMode = TIM_OSSR_DISABLE;
 sBreakDeadTimeConfig.OffStateIDLEMode = TIM_OSSI_DISABLE;
 sBreakDeadTimeConfig.LockLevel = TIM_LOCKLEVEL_OFF;
 sBreakDeadTimeConfig.DeadTime = 0;
 sBreakDeadTimeConfig.BreakState = TIM_BREAK_DISABLE;
 sBreakDeadTimeConfig.BreakPolarity = TIM_BREAKPOLARITY_HIGH;
 sBreakDeadTimeConfig.BreakFilter = 0;
 sBreakDeadTimeConfig.AutomaticOutput = TIM_AUTOMATICOUTPUT_DISABLE;
 if (HAL_TIMEx_ConfigBreakDeadTime(&htim17, &sBreakDeadTimeConfig) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN TIM17_Init 2 */

 /* USER CODE END TIM17_Init 2 */
 HAL_TIM_MspPostInit(&htim17);

}

/**
 * Enable DMA controller clock
 */
static void MX_DMA_Init(void)
{

 /* DMA controller clock enable */
 __HAL_RCC_DMA1_CLK_ENABLE();

 /* DMA interrupt init */
 /* DMA1_Channel1_IRQn interrupt configuration */
 HAL_NVIC_SetPriority(DMA1_Channel1_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(DMA1_Channel1_IRQn);

}

/**
 * @brief GPIO Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_GPIO_Init(void)
{
/* USER CODE BEGIN MX_GPIO_Init_1 */
/* USER CODE END MX_GPIO_Init_1 */

 /* GPIO Ports Clock Enable */
 __HAL_RCC_GPIOF_CLK_ENABLE();
 __HAL_RCC_GPIOA_CLK_ENABLE();

/* USER CODE BEGIN MX_GPIO_Init_2 */
/* USER CODE END MX_GPIO_Init_2 */
}

/* USER CODE BEGIN 4 */

/* USER CODE END 4 */

/**
 * @brief This function is executed in case of error occurrence.
 * @retval None
 */
void Error_Handler(void)
{
 /* USER CODE BEGIN Error_Handler_Debug */
 /* User can add his own implementation to report the HAL error return state */
 __disable_irq();
 while (1)
 {
 }
 /* USER CODE END Error_Handler_Debug */
}

#ifdef USE_FULL_ASSERT
/**
 * @brief Reports the name of the source file and the source line number
 * where the assert_param error has occurred.
 * @PAram file: pointer to the source file name
 * @PAram line: assert_param error line source number
 * @retval None
 */
void assert_failed(uint8_t *file, uint32_t line)
{
 /* USER CODE BEGIN 6 */
 /* User can add his own implementation to report the file name and line number,
 ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
 /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */

 

/* USER CODE BEGIN Header */
/**
 ******************************************************************************
 * @file stm32f3xx_hal_msp.c
 * @brief This file provides code for the MSP Initialization
 * and de-Initialization codes.
 ******************************************************************************
*/
/* Includes ------------------------------------------------------------------*/
#include "main.h"

extern DMA_HandleTypeDef hdma_tim17_ch1_up;

void HAL_TIM_MspPostInit(TIM_HandleTypeDef *htim);
 /**
 * Initializes the Global MSP.
 */
void HAL_MspInit(void)
{

 /* USER CODE BEGIN MspInit 0 */

 /* USER CODE END MspInit 0 */

 __HAL_RCC_SYSCFG_CLK_ENABLE();
 __HAL_RCC_PWR_CLK_ENABLE();

 /* System interrupt init*/

 /* USER CODE BEGIN MspInit 1 */

 /* USER CODE END MspInit 1 */
}

/**
* @brief TIM_Base MSP Initialization
* This function configures the hardware resources used in this example
* @PAram htim_base: TIM_Base handle pointer
* @retval None
*/
void HAL_TIM_Base_MspInit(TIM_HandleTypeDef* htim_base)
{
 if(htim_base->Instance==TIM17)
 {
 /* USER CODE BEGIN TIM17_MspInit 0 */

 /* USER CODE END TIM17_MspInit 0 */
 /* Peripheral clock enable */
 __HAL_RCC_TIM17_CLK_ENABLE();

 /* TIM17 DMA Init */
 /* TIM17_CH1_UP Init */
 hdma_tim17_ch1_up.Instance = DMA1_Channel1;
 hdma_tim17_ch1_up.Init.Direction = DMA_MEMORY_TO_PERIPH;
 hdma_tim17_ch1_up.Init.PeriphInc = DMA_PINC_DISABLE;
 hdma_tim17_ch1_up.Init.MemInc = DMA_MINC_ENABLE;
 hdma_tim17_ch1_up.Init.PeriphDataAlignment = DMA_PDATAALIGN_HALFWORD;
 hdma_tim17_ch1_up.Init.MemDataAlignment = DMA_MDATAALIGN_HALFWORD;
 hdma_tim17_ch1_up.Init.Mode = DMA_CIRCULAR;
 hdma_tim17_ch1_up.Init.Priority = DMA_PRIORITY_HIGH;
 if (HAL_DMA_Init(&hdma_tim17_ch1_up) != HAL_OK)
 {
 Error_Handler();
 }

 /* Several peripheral DMA handle pointers point to the same DMA handle.
 Be aware that there is only one channel to perform all the requested DMAs. */
 __HAL_LINKDMA(htim_base,hdma[TIM_DMA_ID_CC1],hdma_tim17_ch1_up);
 __HAL_LINKDMA(htim_base,hdma[TIM_DMA_ID_UPDATE],hdma_tim17_ch1_up);

 /* TIM17 interrupt Init */
 HAL_NVIC_SetPriority(TIM1_TRG_COM_TIM17_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(TIM1_TRG_COM_TIM17_IRQn);
 /* USER CODE BEGIN TIM17_MspInit 1 */

 /* USER CODE END TIM17_MspInit 1 */
 }

}

void HAL_TIM_MspPostInit(TIM_HandleTypeDef* htim)
{
 GPIO_InitTypeDef GPIO_InitStruct = {0};
 if(htim->Instance==TIM17)
 {
 /* USER CODE BEGIN TIM17_MspPostInit 0 */

 /* USER CODE END TIM17_MspPostInit 0 */

 __HAL_RCC_GPIOA_CLK_ENABLE();
 /**TIM17 GPIO Configuration
 PA7 ------> TIM17_CH1
 */
 GPIO_InitStruct.Pin = GPIO_PIN_7;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 GPIO_InitStruct.Alternate = GPIO_AF1_TIM17;
 HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

 /* USER CODE BEGIN TIM17_MspPostInit 1 */

 /* USER CODE END TIM17_MspPostInit 1 */
 }

}
/**
* @brief TIM_Base MSP De-Initialization
* This function freeze the hardware resources used in this example
* @PAram htim_base: TIM_Base handle pointer
* @retval None
*/
void HAL_TIM_Base_MspDeInit(TIM_HandleTypeDef* htim_base)
{
 if(htim_base->Instance==TIM17)
 {
 /* USER CODE BEGIN TIM17_MspDeInit 0 */

 /* USER CODE END TIM17_MspDeInit 0 */
 /* Peripheral clock disable */
 __HAL_RCC_TIM17_CLK_DISABLE();

 /* TIM17 DMA DeInit */
 HAL_DMA_DeInit(htim_base->hdma[TIM_DMA_ID_CC1]);
 HAL_DMA_DeInit(htim_base->hdma[TIM_DMA_ID_UPDATE]);

 /* TIM17 interrupt DeInit */
 HAL_NVIC_DisableIRQ(TIM1_TRG_COM_TIM17_IRQn);
 /* USER CODE BEGIN TIM17_MspDeInit 1 */

 /* USER CODE END TIM17_MspDeInit 1 */
 }

}

/* USER CODE BEGIN 1 */

/* USER CODE END 1 */

 

 

daded1_3-1715402159278.png

 

 

daded1_4-1715402178719.png

 

daded1_5-1715402229843.png

 

 

    This topic has been closed for replies.

    4 replies

    ST Employee
    May 6, 2024

    Hello @daded.1

    You're on the right track with using HAL_TIM_OC_Start_DMA(), this function allows you to update the CCR with the values provided in the wave_buffer array using DMA and starts the timer in output compare mode.

    In the DMA config, the DMA needs to be set to circular mode to reload the wave_buffer values when it reaches the end automatically.

    Also, you may want to implement HAL_TIM_OC_DelayElapsedCallback to handle the DMA interrupt on each toggle event

    To understand how every function works, you can look at its prototype in the stm32f3xx_hal_tim.c file and read the comments explaining its parameters

    Regarding refreshing your memory, refer to the following links: 

    Description of STM32F3 HAL and low-layer drivers

    STM32CubeMX for STM32 configuration and initialization C code generation

     

    Hope that helps!

     

    daded.1Author
    Visitor II
    May 11, 2024

    Thank you Sarra.S,

    That was very insightful. After reading the manuals and going through the prototypes, I went ahead to enable the timer/dma using 

     

    HAL_TIM_OC_Start_DMA(&htim15, TIM_CHANNEL_1, (uint16_t*)wave_buffer, 5);

     

    I ran the code and I can see the output pin toggle, but it is nothing compared to the expected pulses. On reset, it just toggles at a period of 2 times the set period.

    As for DMA config, I have that set as follows in the CubeMX generated file

     

     /* Peripheral clock enable */
     __HAL_RCC_TIM15_CLK_ENABLE();
    
     /* TIM15 DMA Init */
     /* TIM15_CH1_UP_TRIG_COM Init */
     hdma_tim15_ch1_up_trig_com.Instance = DMA1_Channel5;
     hdma_tim15_ch1_up_trig_com.Init.Direction = DMA_MEMORY_TO_PERIPH;
     hdma_tim15_ch1_up_trig_com.Init.PeriphInc = DMA_PINC_DISABLE;
     hdma_tim15_ch1_up_trig_com.Init.MemInc = DMA_MINC_ENABLE;
     hdma_tim15_ch1_up_trig_com.Init.PeriphDataAlignment = DMA_PDATAALIGN_HALFWORD;
     hdma_tim15_ch1_up_trig_com.Init.MemDataAlignment = DMA_MDATAALIGN_HALFWORD;
     hdma_tim15_ch1_up_trig_com.Init.Mode = DMA_CIRCULAR;
     hdma_tim15_ch1_up_trig_com.Init.Priority = DMA_PRIORITY_HIGH;
     if (HAL_DMA_Init(&hdma_tim15_ch1_up_trig_com) != HAL_OK)
     {
     Error_Handler();
     }

     

    Now, I am not sure if that is all that is necessary since CubeMX has done a lot of the heavy lifting, but do I need to manually set the DMA peripheral/memory base address, direction or buffer size? Also, is there something I could be missing as regards implementing interrupts? I appreciate any help/advise with this.

    Thank you!

    --------------------------------- code below ---------------------------------

    /* USER CODE BEGIN Header */
    /**
     ******************************************************************************
     * @file : main.c
     * @brief : Main program body
     ******************************************************************************
     * @attention
     *
     * Copyright (c) 2024 STMicroelectronics.
     * All rights reserved.
     *
     * This software is licensed under terms that can be found in the LICENSE file
     * in the root directory of this software component.
     * If no LICENSE file comes with this software, it is provided AS-IS.
     *
     ******************************************************************************
     */
    /* USER CODE END Header */
    /* Includes ------------------------------------------------------------------*/
    #include "main.h"
    
    /* Private includes ----------------------------------------------------------*/
    /* USER CODE BEGIN Includes */
    
    /* USER CODE END Includes */
    
    /* Private typedef -----------------------------------------------------------*/
    /* USER CODE BEGIN PTD */
    
    /* USER CODE END PTD */
    
    /* Private define ------------------------------------------------------------*/
    /* USER CODE BEGIN PD */
    
    /* USER CODE END PD */
    
    /* Private macro -------------------------------------------------------------*/
    /* USER CODE BEGIN PM */
    
    /* USER CODE END PM */
    
    /* Private variables ---------------------------------------------------------*/
    TIM_HandleTypeDef htim15;
    DMA_HandleTypeDef hdma_tim15_ch1_up_trig_com;
    
    /* USER CODE BEGIN PV */
    
    /* USER CODE END PV */
    
    /* Private function prototypes -----------------------------------------------*/
    void SystemClock_Config(void);
    static void MX_GPIO_Init(void);
    static void MX_DMA_Init(void);
    static void MX_TIM15_Init(void);
    /* USER CODE BEGIN PFP */
    
    /* USER CODE END PFP */
    
    /* Private user code ---------------------------------------------------------*/
    /* USER CODE BEGIN 0 */
    
    /* USER CODE END 0 */
    
    /**
     * @brief The application entry point.
     * @retval int
     */
    int main(void)
    {
    
     /* USER CODE BEGIN 1 */
     uint16_t wave_buffer[5] = {5700, 3000, 4700, 3000, 10000};
    
     /*
     ___________ ___________ ___________
     | 5700 |___3000___| 4700 |___3000___| 10000 |_________________________
    
     <------------------------------------33ms------------------------------------>
     
     */
     
     /* USER CODE END 1 */
    
     /* MCU Configuration--------------------------------------------------------*/
    
     /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
     HAL_Init();
    
     /* USER CODE BEGIN Init */
    
     /* USER CODE END Init */
    
     /* Configure the system clock */
     SystemClock_Config();
    
     /* USER CODE BEGIN SysInit */
    
     /* USER CODE END SysInit */
    
     /* Initialize all configured peripherals */
     MX_GPIO_Init();
     MX_DMA_Init();
     MX_TIM15_Init();
     /* USER CODE BEGIN 2 */
     HAL_TIM_OC_DelayElapsedCallback(&htim15);
     //enable dma
     HAL_TIM_OC_Start_DMA(&htim15, TIM_CHANNEL_1, (uint16_t*)wave_buffer, 5);
     /* USER CODE END 2 */
    
     /* Infinite loop */
     /* USER CODE BEGIN WHILE */
     while (1)
     {
     /* USER CODE END WHILE */
    
     /* USER CODE BEGIN 3 */
     }
     /* USER CODE END 3 */
    }
    
    /**
     * @brief System Clock Configuration
     * @retval None
     */
    void SystemClock_Config(void)
    {
     RCC_OscInitTypeDef RCC_OscInitStruct = {0};
     RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
    
     /** Initializes the RCC Oscillators according to the specified parameters
     * in the RCC_OscInitTypeDef structure.
     */
     RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
     RCC_OscInitStruct.HSEState = RCC_HSE_ON;
     RCC_OscInitStruct.HSEPredivValue = RCC_HSE_PREDIV_DIV1;
     RCC_OscInitStruct.HSIState = RCC_HSI_ON;
     RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
     RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
     RCC_OscInitStruct.PLL.PLLMUL = RCC_PLL_MUL9;
     if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
     {
     Error_Handler();
     }
    
     /** Initializes the CPU, AHB and APB buses clocks
     */
     RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
     |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
     RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
     RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
     RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV2;
     RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
    
     if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_2) != HAL_OK)
     {
     Error_Handler();
     }
    }
    
    /**
     * @brief TIM15 Initialization Function
     * @PAram None
     * @retval None
     */
    static void MX_TIM15_Init(void)
    {
    
     /* USER CODE BEGIN TIM15_Init 0 */
    
     /* USER CODE END TIM15_Init 0 */
    
     TIM_ClockConfigTypeDef sClockSourceConfig = {0};
     TIM_MasterConfigTypeDef sMasterConfig = {0};
     TIM_OC_InitTypeDef sConfigOC = {0};
     TIM_BreakDeadTimeConfigTypeDef sBreakDeadTimeConfig = {0};
    
     /* USER CODE BEGIN TIM15_Init 1 */
    
     /* USER CODE END TIM15_Init 1 */
     htim15.Instance = TIM15;
     htim15.Init.Prescaler = 72-1; // lower internal clock of 72MHz to 1MHz
     htim15.Init.CounterMode = TIM_COUNTERMODE_UP;
     htim15.Init.Period = 33000; // each full wave period is 33ms
     htim15.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
     htim15.Init.RepetitionCounter = 0;
     htim15.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
     if (HAL_TIM_Base_Init(&htim15) != HAL_OK)
     {
     Error_Handler();
     }
     sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
     if (HAL_TIM_ConfigClockSource(&htim15, &sClockSourceConfig) != HAL_OK)
     {
     Error_Handler();
     }
     if (HAL_TIM_OC_Init(&htim15) != HAL_OK)
     {
     Error_Handler();
     }
     sMasterConfig.MasterOutputTrigger = TIM_TRGO_OC1REF;
     sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
     if (HAL_TIMEx_MasterConfigSynchronization(&htim15, &sMasterConfig) != HAL_OK)
     {
     Error_Handler();
     }
    
     // output compare parameters
     sConfigOC.OCMode = TIM_OCMODE_TOGGLE;
     sConfigOC.Pulse = 0;
     sConfigOC.OCPolarity = TIM_OCPOLARITY_LOW;
     sConfigOC.OCNPolarity = TIM_OCNPOLARITY_HIGH;
     sConfigOC.OCFastMode = TIM_OCFAST_DISABLE;
     sConfigOC.OCIdleState = TIM_OCIDLESTATE_RESET;
     sConfigOC.OCNIdleState = TIM_OCNIDLESTATE_RESET;
     if (HAL_TIM_OC_ConfigChannel(&htim15, &sConfigOC, TIM_CHANNEL_1) != HAL_OK)
     {
     Error_Handler();
     }
     __HAL_TIM_ENABLE_OCxPRELOAD(&htim15, TIM_CHANNEL_1);
     sBreakDeadTimeConfig.OffStateRunMode = TIM_OSSR_DISABLE;
     sBreakDeadTimeConfig.OffStateIDLEMode = TIM_OSSI_DISABLE;
     sBreakDeadTimeConfig.LockLevel = TIM_LOCKLEVEL_OFF;
     sBreakDeadTimeConfig.DeadTime = 0;
     sBreakDeadTimeConfig.BreakState = TIM_BREAK_DISABLE;
     sBreakDeadTimeConfig.BreakPolarity = TIM_BREAKPOLARITY_HIGH;
     sBreakDeadTimeConfig.BreakFilter = 0;
     sBreakDeadTimeConfig.AutomaticOutput = TIM_AUTOMATICOUTPUT_DISABLE;
     if (HAL_TIMEx_ConfigBreakDeadTime(&htim15, &sBreakDeadTimeConfig) != HAL_OK)
     {
     Error_Handler();
     }
     /* USER CODE BEGIN TIM15_Init 2 */
     
     /* USER CODE END TIM15_Init 2 */
     HAL_TIM_MspPostInit(&htim15);
     // connect dma
     HAL_TIM_OC_Start_DMA(&htim15, TIM_CHANNEL_1, &wave_buffer, 5);
    }
    
    /**
     * Enable DMA controller clock
     */
    static void MX_DMA_Init(void)
    {
    
     /* DMA controller clock enable */
     __HAL_RCC_DMA1_CLK_ENABLE();
    
     /* DMA interrupt init */
     /* DMA1_Channel5_IRQn interrupt configuration */
     HAL_NVIC_SetPriority(DMA1_Channel5_IRQn, 0, 0);
     HAL_NVIC_EnableIRQ(DMA1_Channel5_IRQn);
    
     
    
    }
    
    /**
     * @brief GPIO Initialization Function
     * @PAram None
     * @retval None
     */
    static void MX_GPIO_Init(void)
    {
    /* USER CODE BEGIN MX_GPIO_Init_1 */
    /* USER CODE END MX_GPIO_Init_1 */
    
     /* GPIO Ports Clock Enable */
     __HAL_RCC_GPIOF_CLK_ENABLE();
    
    /* USER CODE BEGIN MX_GPIO_Init_2 */
    /* USER CODE END MX_GPIO_Init_2 */
    }
    
    /* USER CODE BEGIN 4 */
    
    /* USER CODE END 4 */
    
    /**
     * @brief This function is executed in case of error occurrence.
     * @retval None
     */
    void Error_Handler(void)
    {
     /* USER CODE BEGIN Error_Handler_Debug */
     /* User can add his own implementation to report the HAL error return state */
     __disable_irq();
     while (1)
     {
     }
     /* USER CODE END Error_Handler_Debug */
    }
    
    #ifdef USE_FULL_ASSERT
    /**
     * @brief Reports the name of the source file and the source line number
     * where the assert_param error has occurred.
     * @PAram file: pointer to the source file name
     * @PAram line: assert_param error line source number
     * @retval None
     */
    void assert_failed(uint8_t *file, uint32_t line)
    {
     /* USER CODE BEGIN 6 */
     /* User can add his own implementation to report the file name and line number,
     ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
     /* USER CODE END 6 */
    }
    #endif /* USE_FULL_ASSERT */

      

    Super User
    May 11, 2024

    I don't use Cube/CubeMX and don't try to understand your code, but IMO you want to do 6 transitions (toggles) per timer period, so you should have:

    - 6 values in the table:

     

    uint16_t wave_buffer[6] = {5700, 3000, 4700, 3000, 10000, 0};

     

    - trigger DMA *only* from the CCx event, *not* from Update event

    JW

    PS. Don't start new thread for the same problem