TIMER Interrupt issue STM32
Hello,
I am facing an issue with my code on my STM32F411
I have a function that is starting a timer TIM5
I want to be able to handle channel 1, Channel 2, Channel 3 interrupt on output compare no output
uint32_t ticks = ms * 10U; /* 10 kHz tick -> 10 ticks per ms */
if (ticks == 0) ticks = 1;
TIM5->CR1 = 0;
TIM5->CR2 = 0;
TIM5->DIER = 0;
TIM5->CCER = 0;
TIM5->CCMR2 = 0; // Channel 3 and 4 CCMR register
// Set prescaler and auto-reload as needed
TIM5->PSC = 96; // No prescaler
TIM5->ARR = 0xFFFF; // Auto-reload max for full range
TIM5->CCMR2 &= ~TIM_CCMR2_CC3S; // CC3S=00 output
TIM5->CCMR2 &= ~TIM_CCMR2_OC3M; // Clear OC3M bits
TIM5->CCMR2 |= (0x3 << TIM_CCMR2_OC3M_Pos); // OC3M=011 toggle mode
// Enable Capture/Compare Channel 3 output (optional for toggling output pins)
TIM5->CCER |= TIM_CCER_CC3E;
// Enable interrupt on Capture/Compare 3 event
TIM5->DIER |= TIM_DIER_CC3IE;
// Enable TIM5 counter
//TIM5->CR1 &= ~TIM_CR1_CEN; // Stop timer while we change ARR/counter
TIM5->ARR = (uint32_t)(ticks - 1U)*10; // Set Auto-reload register
TIM5->CCR3 = (uint32_t)(ticks - 1U)*10; // Channel 2 for marquee update
TIM5->CNT = 0;
//HAL_TIM_Base_Start_IT(&htim5);
/* Enable update interrupt and start one-shot timer */
//TIM5->CR1 |= TIM_CR1_OPM; // One pulse mode
TIM5->DIER |= TIM_DIER_CC3IE; // Enable interrupt on
TIM5->CR1 |= TIM_CR1_CEN; // Start the timer
I configured only Channel 3
And this is my IRQ handler
void TIM5_IRQHandler(void){
//log_info("A");
if (TIM5->SR & TIM_SR_UIF){
TIM5->SR &= ~TIM_SR_UIF; // Clear the overflow interrupt
}
else if (TIM5->SR & TIM_SR_CC1IF){ // Pulse compare interrrupt on Channel 1
TIM5->SR &= ~TIM_SR_CC1IF;
TIM1->CCER &= ~TIM_CCER_CC2NE;
printf("i\n");
flgSoundEffectActive=0;
/* Disable timer and its update interrupt */
//TIM5->CR1 &= ~TIM_CR1_CEN;
/* Disable update interrupt using timer register (clear UIE in DIER) */
//TIM5->DIER &= ~TIM_DIER_UIE;
TIM5->DIER &= ~TIM_DIER_CC1IE;
// Clear the compare interrupt flag
}
else if (TIM5->SR & TIM_SR_CC2IF){
TIM5->SR &= ~TIM_SR_CC2IF;
flgUpdateMarquee=1;
printf("h\n");
}
else if (TIM5->SR & TIM_SR_CC3IF){
TIM5->SR &= ~TIM_SR_CC3IF;
flgUpdateMarquee=1;
printf("j\n");
}
else
TIM5->SR = 0;
}I received the 3 interrupt instead of only the Channel 3
What do I need to change to be able start the timer5 only with a predifined channel
thanks for your help
Vincent