TIMER SYSCHRONISATION
I am using STM32F446RE microcontroller and using MATLAB to develop the logic. Upon launching StmCubeMx, I have kept the clock frequency as 90MHz and 10% duty cycle for TIM1, TIM2, TIM3. So, it gives same output frequency of the pulses (PWM_Output.png) from each PWM. Model screenshot is also attached (model.PNG). All 3 timer settings have been kept same as shown in (Timer_setting.PNG). I want all the 3 pulses shall be in phase. How can I achieve that?
Hoping to hear soon!
Thanks in advance!