To know the Register value to read ADC Converted Data
I am writing the code to read the ADC data from internal temp sensor and ADC.
I want to know that what is the register value to read the ADC data from there.
I am using STM32H743ZIT6 Micro controller. We are using ADC3,
The ADC is set to 16-bit resolution mode
The ADC input clock is 64 MHz. The Clock Prescaler is set to 128. The sampling time for each input is set to 810.5
REgards
Saranraj