Touch sensor with reversed side STM32F429I-DISC1 (touch being detected on the opposite side that was pressed)
Hello.
I purchased a Discovery STM32F429-DISC1 development board to start applications involving LCD screen. However, I am having a problem with the touch sensor. I recorded on the board some applications that I developed with TouchGFX, simple applications like pressing a button and making an image disappear and reappear, the problem is as if the touch sensor was inverted, for example, to press a button on the lower side of the screen I have to touch the top corner of the screen..it's like the sides are reversed..I thought it might be a problem related to my application so I recorded an example provided by ST. I saved the .HEX file and the problem persisted..does anyone have any suggestions on what is happening?
Thanks