trigger ADC exactly at midpoint of PWM ON time in Center-Aligned PWM Mode 2 (TIM1)?

(I'm using NUCLEO-F103RB)
Hello,
I'm currently working on a BLDC motor control project using STM32CubeMX and STM32CubeIDE with STM32 TIM1 peripheral.
I have configured TIM1 in Center-Aligned PWM Mode 2, with:
Prescaler = 3
ARR = 899
So, PWM frequency is 10kHz (from a 72MHz system clock).
In this mode, since the counter counts up and down between 0 and ARR, the counter reaching ARR marks the exact midpoint of the PWM ON time.
I would like to trigger an ADC conversion exactly at that point (i.e., at 50% of the ON time).
To do this, I thought of using TRGO = Update Event, since the update event happens when CNT = ARR in Center-Aligned Mode 2.
However, I am not fully sure if this is guaranteed to occur at that midpoint and whether it's the most precise method.
:question_mark:My questions are:
Is TRGO = Update Event guaranteed to occur exactly when CNT = ARR in Center-Aligned Mode 2?
Is this the best practice to trigger ADC at the center of the PWM ON duration?
If not, is there a more accurate or recommended method?
Any insight or clarification would be greatly appreciated.
Thank you in advance!