Trigger SPI6 DMA transfer using external pin via DMAMUX
Hello,
I'm working with the STM32H723 and need to interface with an external ADC that provides a DRDY (PG2 pin) signal. I'd like to initiate an SPI transfer via DMA whenever the DRDY pin goes low. The ADC is connected to SPI6, and I understand that only BDMA can be used with this peripheral.
My main question is:
How can I configure DMAMUX to trigger a BDMA transfer for SPI6 when the DRDY pin goes low?
I'm using STM32CubeMX for configuration. I’ve looked through existing forum posts and the STM documentation, but haven’t found a clear example or explanation for this setup. Any guidance, examples, or tips to get started would be greatly appreciated.
Thanks in advance!