UART how the overflow works ?
Hello !
I've been wondering, how UART works in receiving side ? I have like maybe 4/5 questions ?
-> What if I have a RX buffer that is full ? The flag is on and I didn't read the data. Then the new data comes after sometime, will it overwrite my data and still the flag will be on ?
-> Is the data in the RX buffer loaded bit after bit or is it loaded whole word (8 bits) in one go and not bit by bit ?
-> How do I know when I type HAL_UART_Transmit and after that the peripheral will be sending data and after transmit command I have the command HAL_UART_Receive, so how do I know it was fast enough to read the whole data without loosing any new or old data ? Like it was to late although the commands were one after another.
-> What if I used IT or DMA, they are non blocking, and questions like above like what if I type Transmit and Receive will I make it in time ? or what if I didn't read data and the buffer sets the flag and new data comes.
These questions came out of curiosity because I read something about how UARTs looks like conceptually but I wondered how it looks like in practice. Because there are many types of commands in UART and wondered "what if" stuff. Also I know that RX works all the time and not only when I type HAL_UART_Receive so I wondered how it works when I have full data or when I type HAL_UART_Receive after HAL_UART_Transmit, will it be fast enough to read full buffor because this Receive commands reads full buffors and not bit by bit data. And what if I type HAL_UART_Receive after some time .. Yea I didn't know how to check it so maybe asking here won't be a problem ;> Sorry if it is.