UART pins issue rx, tx & enable gets high after transmittting data properly for hours.
Hi community,
I am getting error in my stm32 microcontroller system which is used to communicate data of the sensor uart.
Initially everything is working fine the adc data is coming perfect. Able to send data through uart without any error. But after 1 to 2 hour of communication through uart rx, tx & enable pins are getting stuck to high. Not able to transmit data. At that very moment data through adc is been fetched & displayed by the controller as required only issue is the pins are not getting to low state after transmitting data. Please help & let us know if you have any particular solution or recommendation.