uart request response just during debug and debugger connected
Hello people,
I have been developing a firmware to be used in the stm32g051. One of the features is the ability to respon to request to get information from the uC. I used dma for the uart1 tx and rx. I was happily developing and testing the new feature added into the stm32g051. Then when I use it without the debugger, it is unable to stablish communications between the PC and the microcontroller.
The curious thing is the fact that I remove the debugger -I disconnect it- and the communication still works. It is the "reset" without debugger what is unable to stablish the connection.
I change the clocks following the several post regarding this problem but the solution still eludes me.