Skip to main content
Visitor II
August 29, 2024
Solved

UART Transmission on STM32 Nucleo-h723zg

  • August 29, 2024
  • 2 replies
  • 1992 views

 

I am using STM32 Nucleo-h723zg for a UART serial transmission using UART4 and UART7. I have used UART4 only in my code to test since using both was not working. Still, nothing is showing on my RealTerm serial monitor. I used STM32 Cube IDE. I don't know why I can't see data being transmitted on the serial monitor.

 

/* USER CODE BEGIN Header */
/**
 ******************************************************************************
 * @file : main.c
 * @brief : Main program body
 ******************************************************************************
 * @attention
 *
 * Copyright (c) 2024 STMicroelectronics.
 * All rights reserved.
 *
 * This software is licensed under terms that can be found in the LICENSE file
 * in the root directory of this software component.
 * If no LICENSE file comes with this software, it is provided AS-IS.
 *
 ******************************************************************************
 */
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"

/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */

/* USER CODE END Includes */

/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */

/* USER CODE END PTD */

/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */

/* USER CODE END PD */

/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */

/* USER CODE END PM */

/* Private variables ---------------------------------------------------------*/

UART_HandleTypeDef huart4;
UART_HandleTypeDef huart7;

/* USER CODE BEGIN PV */

/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_UART4_Init(void);
static void MX_UART7_Init(void);
/* USER CODE BEGIN PFP */

/* USER CODE END PFP */

/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */

/* USER CODE END 0 */

/**
 * @brief The application entry point.
 * @retval int
 */
uint8_t buffer_uart[] = "Hello world";
int main(void)
{

 /* USER CODE BEGIN 1 */

 /* USER CODE END 1 */

 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();

 /* USER CODE BEGIN Init */

 /* USER CODE END Init */

 /* Configure the system clock */
 SystemClock_Config();

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_UART4_Init();
 MX_UART7_Init();
 /* USER CODE BEGIN 2 */

 /* USER CODE END 2 */

 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {
 /* USER CODE END WHILE */
	 HAL_UART_Transmit(&huart4, buffer_uart, sizeof(buffer_uart), 100);
	 HAL_Delay(10);
 /* USER CODE BEGIN 3 */
 }
 /* USER CODE END 3 */
}

/**
 * @brief System Clock Configuration
 * @retval None
 */
void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

 /** Supply configuration update enable
 */
 HAL_PWREx_ConfigSupply(PWR_LDO_SUPPLY);

 /** Configure the main internal regulator output voltage
 */
 __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE2);

 while(!__HAL_PWR_GET_FLAG(PWR_FLAG_VOSRDY)) {}

 /** Initializes the RCC Oscillators according to the specified parameters
 * in the RCC_OscInitTypeDef structure.
 */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
 RCC_OscInitStruct.HSIState = RCC_HSI_DIV1;
 RCC_OscInitStruct.HSICalibrationValue = 64;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
 RCC_OscInitStruct.PLL.PLLM = 4;
 RCC_OscInitStruct.PLL.PLLN = 12;
 RCC_OscInitStruct.PLL.PLLP = 1;
 RCC_OscInitStruct.PLL.PLLQ = 4;
 RCC_OscInitStruct.PLL.PLLR = 2;
 RCC_OscInitStruct.PLL.PLLRGE = RCC_PLL1VCIRANGE_3;
 RCC_OscInitStruct.PLL.PLLVCOSEL = RCC_PLL1VCOWIDE;
 RCC_OscInitStruct.PLL.PLLFRACN = 0;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }

 /** Initializes the CPU, AHB and APB buses clocks
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2
 |RCC_CLOCKTYPE_D3PCLK1|RCC_CLOCKTYPE_D1PCLK1;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
 RCC_ClkInitStruct.SYSCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_HCLK_DIV2;
 RCC_ClkInitStruct.APB3CLKDivider = RCC_APB3_DIV2;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_APB1_DIV2;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_APB2_DIV2;
 RCC_ClkInitStruct.APB4CLKDivider = RCC_APB4_DIV2;

 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_1) != HAL_OK)
 {
 Error_Handler();
 }
}

/**
 * @brief UART4 Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_UART4_Init(void)
{

 /* USER CODE BEGIN UART4_Init 0 */

 /* USER CODE END UART4_Init 0 */

 /* USER CODE BEGIN UART4_Init 1 */

 /* USER CODE END UART4_Init 1 */
 huart4.Instance = UART4;
 huart4.Init.BaudRate = 115200;
 huart4.Init.WordLength = UART_WORDLENGTH_8B;
 huart4.Init.StopBits = UART_STOPBITS_1;
 huart4.Init.Parity = UART_PARITY_NONE;
 huart4.Init.Mode = UART_MODE_TX_RX;
 huart4.Init.HwFlowCtl = UART_HWCONTROL_NONE;
 huart4.Init.OverSampling = UART_OVERSAMPLING_16;
 huart4.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
 huart4.Init.ClockPrescaler = UART_PRESCALER_DIV1;
 huart4.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
 if (HAL_UART_Init(&huart4) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_UARTEx_SetTxFifoThreshold(&huart4, UART_TXFIFO_THRESHOLD_1_8) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_UARTEx_SetRxFifoThreshold(&huart4, UART_RXFIFO_THRESHOLD_1_8) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_UARTEx_DisableFifoMode(&huart4) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN UART4_Init 2 */

 /* USER CODE END UART4_Init 2 */

}

/**
 * @brief UART7 Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_UART7_Init(void)
{

 /* USER CODE BEGIN UART7_Init 0 */

 /* USER CODE END UART7_Init 0 */

 /* USER CODE BEGIN UART7_Init 1 */

 /* USER CODE END UART7_Init 1 */
 huart7.Instance = UART7;
 huart7.Init.BaudRate = 115200;
 huart7.Init.WordLength = UART_WORDLENGTH_8B;
 huart7.Init.StopBits = UART_STOPBITS_1;
 huart7.Init.Parity = UART_PARITY_NONE;
 huart7.Init.Mode = UART_MODE_TX_RX;
 huart7.Init.HwFlowCtl = UART_HWCONTROL_NONE;
 huart7.Init.OverSampling = UART_OVERSAMPLING_16;
 huart7.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
 huart7.Init.ClockPrescaler = UART_PRESCALER_DIV1;
 huart7.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
 if (HAL_UART_Init(&huart7) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_UARTEx_SetTxFifoThreshold(&huart7, UART_TXFIFO_THRESHOLD_1_8) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_UARTEx_SetRxFifoThreshold(&huart7, UART_RXFIFO_THRESHOLD_1_8) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_UARTEx_DisableFifoMode(&huart7) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN UART7_Init 2 */

 /* USER CODE END UART7_Init 2 */

}

/**
 * @brief GPIO Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_GPIO_Init(void)
{
/* USER CODE BEGIN MX_GPIO_Init_1 */
/* USER CODE END MX_GPIO_Init_1 */

 /* GPIO Ports Clock Enable */
 __HAL_RCC_GPIOF_CLK_ENABLE();
 __HAL_RCC_GPIOA_CLK_ENABLE();

/* USER CODE BEGIN MX_GPIO_Init_2 */
/* USER CODE END MX_GPIO_Init_2 */
}

/* USER CODE BEGIN 4 */

/* USER CODE END 4 */

/**
 * @brief This function is executed in case of error occurrence.
 * @retval None
 */
void Error_Handler(void)
{
 /* USER CODE BEGIN Error_Handler_Debug */
 /* User can add his own implementation to report the HAL error return state */
 __disable_irq();
 while (1)
 {
 }
 /* USER CODE END Error_Handler_Debug */
}

#ifdef USE_FULL_ASSERT
/**
 * @brief Reports the name of the source file and the source line number
 * where the assert_param error has occurred.
 * @PAram file: pointer to the source file name
 * @PAram line: assert_param error line source number
 * @retval None
 */
void assert_failed(uint8_t *file, uint32_t line)
{
 /* USER CODE BEGIN 6 */
 /* User can add his own implementation to report the file name and line number,
 ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
 /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */

 

 

 

    This topic has been closed for replies.
    Best answer by mƎALLEm

    Hello,

    According to the board's schematics you need to use USART3 (Tx: PD8 and Rx: PD9) and use the virtual comport over STL-Link.

    SofLit_0-1724931318953.png

    Unless you have a specific HW connected between UART4 or UART7 and your PC.

     

    2 replies

    mƎALLEmAnswer
    Technical Moderator
    August 29, 2024

    Hello,

    According to the board's schematics you need to use USART3 (Tx: PD8 and Rx: PD9) and use the virtual comport over STL-Link.

    SofLit_0-1724931318953.png

    Unless you have a specific HW connected between UART4 or UART7 and your PC.

     

    SAWAuthor
    Visitor II
    August 29, 2024

    I have changed my code a bit and used USART3 but still no result on the serial monitor

    /* USER CODE BEGIN Header */
    /**
     ******************************************************************************
     * @file : main.c
     * @brief : Main program body
     ******************************************************************************
     * @attention
     *
     * Copyright (c) 2024 STMicroelectronics.
     * All rights reserved.
     *
     * This software is licensed under terms that can be found in the LICENSE file
     * in the root directory of this software component.
     * If no LICENSE file comes with this software, it is provided AS-IS.
     *
     ******************************************************************************
     */
    /* USER CODE END Header */
    /* Includes ------------------------------------------------------------------*/
    #include "main.h"
    
    /* Private includes ----------------------------------------------------------*/
    /* USER CODE BEGIN Includes */
    
    /* USER CODE END Includes */
    
    /* Private typedef -----------------------------------------------------------*/
    /* USER CODE BEGIN PTD */
    
    /* USER CODE END PTD */
    
    /* Private define ------------------------------------------------------------*/
    /* USER CODE BEGIN PD */
    
    /* USER CODE END PD */
    
    /* Private macro -------------------------------------------------------------*/
    /* USER CODE BEGIN PM */
    
    /* USER CODE END PM */
    
    /* Private variables ---------------------------------------------------------*/
    
    UART_HandleTypeDef huart3;
    DMA_HandleTypeDef hdma_usart3_rx;
    
    /* USER CODE BEGIN PV */
    
    /* USER CODE END PV */
    
    /* Private function prototypes -----------------------------------------------*/
    void SystemClock_Config(void);
    static void MX_GPIO_Init(void);
    static void MX_DMA_Init(void);
    static void MX_USART3_UART_Init(void);
    /* USER CODE BEGIN PFP */
    
    /* USER CODE END PFP */
    
    /* Private user code ---------------------------------------------------------*/
    /* USER CODE BEGIN 0 */
    uint8_t buffer_uart[] = "Hello world";
    /* USER CODE END 0 */
    
    /**
     * @brief The application entry point.
     * @retval int
     */
    int main(void)
    {
    
     /* USER CODE BEGIN 1 */
    
     /* USER CODE END 1 */
    
     /* MCU Configuration--------------------------------------------------------*/
    
     /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
     HAL_Init();
    
     /* USER CODE BEGIN Init */
    
     /* USER CODE END Init */
    
     /* Configure the system clock */
     SystemClock_Config();
    
     /* USER CODE BEGIN SysInit */
    
     /* USER CODE END SysInit */
    
     /* Initialize all configured peripherals */
     MX_GPIO_Init();
     MX_DMA_Init();
     MX_USART3_UART_Init();
     /* USER CODE BEGIN 2 */
    
     /* USER CODE END 2 */
    
     /* Infinite loop */
     /* USER CODE BEGIN WHILE */
     while (1)
     {
     /* USER CODE END WHILE */
    	 HAL_UART_Transmit(&huart3,buffer_uart, sizeof(buffer_uart), 100);
     /* USER CODE BEGIN 3 */
     }
     /* USER CODE END 3 */
    }
    
    /**
     * @brief System Clock Configuration
     * @retval None
     */
    void SystemClock_Config(void)
    {
     RCC_OscInitTypeDef RCC_OscInitStruct = {0};
     RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
    
     /** Supply configuration update enable
     */
     HAL_PWREx_ConfigSupply(PWR_LDO_SUPPLY);
    
     /** Configure the main internal regulator output voltage
     */
     __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE2);
    
     while(!__HAL_PWR_GET_FLAG(PWR_FLAG_VOSRDY)) {}
    
     /** Initializes the RCC Oscillators according to the specified parameters
     * in the RCC_OscInitTypeDef structure.
     */
     RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
     RCC_OscInitStruct.HSIState = RCC_HSI_DIV1;
     RCC_OscInitStruct.HSICalibrationValue = 64;
     RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
     RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
     RCC_OscInitStruct.PLL.PLLM = 4;
     RCC_OscInitStruct.PLL.PLLN = 12;
     RCC_OscInitStruct.PLL.PLLP = 1;
     RCC_OscInitStruct.PLL.PLLQ = 4;
     RCC_OscInitStruct.PLL.PLLR = 2;
     RCC_OscInitStruct.PLL.PLLRGE = RCC_PLL1VCIRANGE_3;
     RCC_OscInitStruct.PLL.PLLVCOSEL = RCC_PLL1VCOWIDE;
     RCC_OscInitStruct.PLL.PLLFRACN = 0;
     if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
     {
     Error_Handler();
     }
    
     /** Initializes the CPU, AHB and APB buses clocks
     */
     RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
     |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2
     |RCC_CLOCKTYPE_D3PCLK1|RCC_CLOCKTYPE_D1PCLK1;
     RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
     RCC_ClkInitStruct.SYSCLKDivider = RCC_SYSCLK_DIV1;
     RCC_ClkInitStruct.AHBCLKDivider = RCC_HCLK_DIV2;
     RCC_ClkInitStruct.APB3CLKDivider = RCC_APB3_DIV2;
     RCC_ClkInitStruct.APB1CLKDivider = RCC_APB1_DIV2;
     RCC_ClkInitStruct.APB2CLKDivider = RCC_APB2_DIV2;
     RCC_ClkInitStruct.APB4CLKDivider = RCC_APB4_DIV2;
    
     if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_1) != HAL_OK)
     {
     Error_Handler();
     }
    }
    
    /**
     * @brief USART3 Initialization Function
     * @PAram None
     * @retval None
     */
    static void MX_USART3_UART_Init(void)
    {
    
     /* USER CODE BEGIN USART3_Init 0 */
    
     /* USER CODE END USART3_Init 0 */
    
     /* USER CODE BEGIN USART3_Init 1 */
    
     /* USER CODE END USART3_Init 1 */
     huart3.Instance = USART3;
     huart3.Init.BaudRate = 115200;
     huart3.Init.WordLength = UART_WORDLENGTH_8B;
     huart3.Init.StopBits = UART_STOPBITS_1;
     huart3.Init.Parity = UART_PARITY_NONE;
     huart3.Init.Mode = UART_MODE_TX_RX;
     huart3.Init.HwFlowCtl = UART_HWCONTROL_NONE;
     huart3.Init.OverSampling = UART_OVERSAMPLING_16;
     huart3.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
     huart3.Init.ClockPrescaler = UART_PRESCALER_DIV1;
     huart3.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
     if (HAL_UART_Init(&huart3) != HAL_OK)
     {
     Error_Handler();
     }
     if (HAL_UARTEx_SetTxFifoThreshold(&huart3, UART_TXFIFO_THRESHOLD_1_8) != HAL_OK)
     {
     Error_Handler();
     }
     if (HAL_UARTEx_SetRxFifoThreshold(&huart3, UART_RXFIFO_THRESHOLD_1_8) != HAL_OK)
     {
     Error_Handler();
     }
     if (HAL_UARTEx_DisableFifoMode(&huart3) != HAL_OK)
     {
     Error_Handler();
     }
     /* USER CODE BEGIN USART3_Init 2 */
    
     /* USER CODE END USART3_Init 2 */
    
    }
    
    /**
     * Enable DMA controller clock
     */
    static void MX_DMA_Init(void)
    {
    
     /* DMA controller clock enable */
     __HAL_RCC_DMA1_CLK_ENABLE();
    
     /* DMA interrupt init */
     /* DMA1_Stream0_IRQn interrupt configuration */
     HAL_NVIC_SetPriority(DMA1_Stream0_IRQn, 0, 0);
     HAL_NVIC_EnableIRQ(DMA1_Stream0_IRQn);
    
    }
    
    /**
     * @brief GPIO Initialization Function
     * @PAram None
     * @retval None
     */
    static void MX_GPIO_Init(void)
    {
    /* USER CODE BEGIN MX_GPIO_Init_1 */
    /* USER CODE END MX_GPIO_Init_1 */
    
     /* GPIO Ports Clock Enable */
     __HAL_RCC_GPIOB_CLK_ENABLE();
    
    /* USER CODE BEGIN MX_GPIO_Init_2 */
    /* USER CODE END MX_GPIO_Init_2 */
    }
    
    /* USER CODE BEGIN 4 */
    
    /* USER CODE END 4 */
    
    /**
     * @brief This function is executed in case of error occurrence.
     * @retval None
     */
    void Error_Handler(void)
    {
     /* USER CODE BEGIN Error_Handler_Debug */
     /* User can add his own implementation to report the HAL error return state */
     __disable_irq();
     while (1)
     {
     }
     /* USER CODE END Error_Handler_Debug */
    }
    
    #ifdef USE_FULL_ASSERT
    /**
     * @brief Reports the name of the source file and the source line number
     * where the assert_param error has occurred.
     * @PAram file: pointer to the source file name
     * @PAram line: assert_param error line source number
     * @retval None
     */
    void assert_failed(uint8_t *file, uint32_t line)
    {
     /* USER CODE BEGIN 6 */
     /* User can add his own implementation to report the file name and line number,
     ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
     /* USER CODE END 6 */
    }
    #endif /* USE_FULL_ASSERT */

     

    Technical Moderator
    August 29, 2024

    What GPIOs you selected for UART3? SB12 and SB19 are soldered?

    Did you select the same UART parameters for USART3 as you did for the terminal?

    See also this thread: https://community.st.com/t5/stm32-mcus-products/stm32-nucleo-h7a3zi-board-uart-issue/m-p/712867

    SAWAuthor
    Visitor II
    September 2, 2024

    I managed to do the UART transceiving. Only the USART3 was working. I had to change the data type from a string to a buffer for the STM32h723zg. The string format was working when I used stm32 nucleo C031C6. What is the reason behind this?

    Thank you for your help this far.