Unable to activate LWIP on STM32H757IIT6
I am not able to activate LWIP middleware for M7 core on any dualcore STM32. (I am able to do it on single-core devices and already have LWIP working on H743 Nucleo)
Steps I have done (exactly in this order):
- create a new project for STM32H757IITx in CubeIDE
- agree usage of default configuration of speculation processing
- enable SYS -> Cortex_M7 -> I cache
- enable SYS -> Cortex_M7 -> D cache
- enable ETH and configure it for M7 core with RMII
- enable FreeRTOS_M7
- enable LWIP for Cortex M7 in the sidebar.
Now I can see the second bar for LWIP. Runtime context M7 is checked but it is not possible to check "enable" checkbox to activate LWIP. When I put the mouse on the enable checkbox, I can see a warning that "D-cache must be enabled on M7 to use LWIP". But the problem is that D-cache is already enabled. It seems to me like a bug in IDE because I am able to activate it on singlecore devices with the exactly same steps. It also works on M4 core on dualcore H757.
I found partial workaround using working example from ST member and manually editing IOC file to fit H757 LQFP instead of H747 BGA but this is not a nice solution and it sometimes create problems when regenerating code.
Thank you