Unable to Connect to NUCLEO-STM32H7S3L8 in STM32CubeProgrammer or STM32CubeIDE
Hello all,
I am working with a NUCLEO-STM32H7S3L8 board, but I am unable to connect to it using STM32CubeProgrammer or flash firmware using STM32CubeIDE. However, I am still able to update the board’s firmware successfully.
Possible Cause:
I suspect that I might have pressed the reset button while flashing firmware to the device, which could have caused the issue.
Issue:
- Unable to connect to the board via STM32CubeProgrammer
- Unable to flash firmware in STM32CubeIDE
- I cannot perform a hard reset because it requires a connection in STM32CubeProgrammer
Question:
What steps can I take to recover my board and regain access?
Any help or suggestions would be greatly appreciated.
Thank you!!