Unable to Debug or Connect STM32L562E-DK After Enabling Read Protection
Hi,
I am facing an issue with my STM32L562E-DK board. Initially, I was able to debug it using STM32CubeIDE. However, after attempting to configure the controller in UART boot mode, I accidentally enabled read protection (DC:LEVEL 1). Since then, I cannot debug the board or connect to it using STM32CubeProgrammer.
Whenever I try to connect the controller via STM32CubeProgrammer, it fails to establish a connection. I suspect something went wrong during the configuration.
I have attached an image below showing the error that occurs when I try to connect.

How can I resolve this issue and regain access to my controller?
Edited by ST Moderator to correct the board name STM32L562E-DK (instead STM32L62E-DK)