Unable to flash or debug STM32L432KCU at 3.3v, but works at 2.2v?
Hello,
I have an STM32L432KCU chip that's on a custom board. I have exposed SWD pins for debugging and flashing. Currently I'm only able to flash and debug the chip if I supply the STM with 2.2v from my external power supply. If I run the STM at the standard 3.3v, I get the "No STM3 target found" message when using CubeIDE, plus running CubeProgrammer, I also cannot connect to the STM to read the flash contents but can at 2.2v. These are fresh chips with no previous firmware flashed onto them, so I don't believe they should be in low power mode. Even if they happen to be in low power mode from the factory, I flash them at 2.2v with a default program to ensure they aren't running in a low power mode.
After flashing the chip at 2.2v, I can supply the normal 3.3v and the chip runs just fine. However, for me to debug or flash new firmware, I can only get it to run at 2.2v. Any ideas?