Unable to read second ADC channel
Hi,
I am using STM32F030 for a project where I need to trigger ADC conversion every 100us. I am running this SoC on 8MHz HSI. I am using TIM3 TRG for initiating ADC conversion every 100us. I am obtain ADC every 100us with ADC_CH5 which is set to 3V3 and getting result in 4024 decimals. But I am unable to get readings from ADC_CH7 which is set to GND and I always get same reading as of ADC_CH5.
May be I am not correctly configuring ADC_CH7 or there is an issue in interrupt handling. I have attached my code for your ready reference please.
ADC Configuration:
void adc_tg0_init(void)
{
// Enable Clock to GPIOA
RCC->AHBENR |= GPIOA_EN;
// PA5 as analog input
GPIOA->MODER |= (1U<<10);
GPIOA->MODER |= (1U<<11);
// PA7 as analog input
GPIOA->MODER |= (1U<<14);
GPIOA->MODER |= (1U<<15);
// Enable Clock to ADC
RCC->APB2ENR |= ADC_EN;
// Enable external trigger on rising edge
ADC1->CFGR1 |= (1U<<10);
ADC1->CFGR1 &= ~(1U<<11);
// Select Timer 3 TRG0 [TRG3] event as external trigger
ADC1->CFGR1 |= (1U<<6);
ADC1->CFGR1 |= (1U<<7);
ADC1->CFGR1 &= ~(1U<<8);
/* ADC Enable Procedure */
if ((ADC1->ISR & ADC_ISR_ADRDY) != 0)
{
ADC1->ISR |= ADC_ISR_ADRDY;
}
ADC1->CR |= ADC_CR_ADEN;
while ((ADC1->ISR & ADC_ISR_ADRDY) ==0) {}
/* Channel Selection */
ADC1->CHSELR |= ADC_CHSELR_CHSEL5 | ADC_CHSELR_CHSEL7;
/* Sampling Mode Selection */
ADC1->SMPR |= ADC_SMPR_SMP_1 |
ADC_SMPR_SMP_2;
/* Enable Interrupts */
ADC1->IER = ADC_IER_EOCIE | ADC_IER_EOSEQIE |
ADC_IER_OVRIE;
/* Set/ Enable VRef to Internal */
ADC->CCR |= ADC_CCR_VREFEN;
/* Enable NVIC */
NVIC_EnableIRQ(ADC1_COMP_IRQn);
// Start ADC
ADC1->CR |= ADC_CR_ADSTART;
// Start Timer 3
TIM3->CR1 |= TIM_CR1_CEN;
}
ADC Interrupt:
void ADC_IRQHandler(void)
{
if (ADC1->ISR & ADC_ISR_EOC)
{
adc_raw_data[adc_idx] = ADC1->DR;
adc_idx++;
pa6_toggle();
ADC1->ISR |= ADC_ISR_EOC;
}
if (ADC1->ISR & ADC_ISR_EOSEQ)
{
ADC1->ISR |= ADC_ISR_EOSEQ;
}
if (ADC1->ISR & ADC_ISR_OVR)
{
adc_ovr = true;
ADC1->ISR |= ADC_ISR_OVR;
}
}
Regards