Unable to receive messages from USB CAN Analyzer to STM32F407 Discovery board.
Hello,
I am trying to send the message from my USB-CAN Analyzer to my board STM32F407 discovery board, but I am unable to do that.
HAL_CAN_GetRxMessage(&hcan1, CAN_RX_FIFO0, &rx_header, rx_data);
// Process received message
handleReceivedMessage(&rx_header, rx_data);
This is my function to read message.
void handleReceivedMessage(CAN_RxHeaderTypeDef *rx_header, uint8_t *rx_data)
{
// Your custom handling of received message
// Example: LED blinking based on received data
HAL_GPIO_TogglePin(GPIOB, GPIO_PIN_12); // Toggle LED
}
This is my handlereceivedMessage function.
Below is my message which I am sending from USB-CAN Analyzer.
Best Regards
Rohit Kumar