Unable to regress to RDP=0
I'm working on a custom STM32U5 board and I'm trying to harden the system.
I followed the AN5347 (https://www.st.com/resource/en/application_note/an5347-arm-trustzone-features-for-stm32l5-and-stm32u5-series-stmicroelectronics.pdf) in particular I followed the chapter 10 with success as I was able to raise up to RDP=2 with OEM password and back to RDP=0.
Then I tried for the second time using the STM32CubeProgrammer instead of the command line as described in the application note, but I got some issues at step 5: Set RDP level 2. The STM32CubeProgrammer did not end the process and got stuck writing RDP=0xCC in the option byte and after ten minutes I forced the termination of the GUI.
After that I was not able to recover to RDP=0.
Every time I try to send a command to the board I get some error.
If I try to follow chapter 10.6 Unlock RDP level 2 with OEM2Key with the command line:
STM32_Programmer_CLI.exe -c port=swd mode=UR -unlockrdp2 0xMYKEYLOW 0xMYKEYHIthe result is the following:
-------------------------------------------------------------------
STM32CubeProgrammer v2.13.0
-------------------------------------------------------------------
ST-LINK SN : 53FF71068389505253152567
ST-LINK FW : V2J40S7
Board : --
Voltage : 3.39V
Unlock RDP2 password succefully done!
Error: ST-LINK error (DEV_TARGET_NOT_HALTED)All other commands sent via cli or via the programmer, get some error, most of the time unable to read values.
Now I don't know what to do to recover this board.
Any idea?